2021-02-05 12:09 PM
Hi,
I'm running into a very strange issue with the CAN module. When enabling ABOM on CAN2, some but not all of the FIFO1 RX interrupts are missed. As soon as I disable the ABOM setting, everything works as expected. Has anyone seen this behavior before? For reference, here's my configuration code:
void InitializeCAN() {
CAN_FilterTypeDef sFilterConfig;
//hcan1
hcan1.Instance = CAN1;
hcan1.Init.Prescaler = 6;
hcan1.Init.Mode = CAN_MODE_NORMAL;
hcan1.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan1.Init.TimeSeg1 = CAN_BS1_11TQ;
hcan1.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan1.Init.TimeTriggeredMode = DISABLE;
hcan1.Init.AutoBusOff = ENABLE;
hcan1.Init.AutoWakeUp = DISABLE;
hcan1.Init.AutoRetransmission = ENABLE;
hcan1.Init.ReceiveFifoLocked = DISABLE;
hcan1.Init.TransmitFifoPriority = DISABLE;
HAL_CAN_Init(&hcan1);
sFilterConfig.FilterIdHigh = (0x28A << 5);
sFilterConfig.FilterIdLow = (0x28A << 5);
sFilterConfig.FilterMaskIdHigh = (0x700<< 5);
sFilterConfig.FilterMaskIdLow = (0x700<< 5);
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_16BIT;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.FilterBank = 0;
sFilterConfig.SlaveStartFilterBank = 14;
HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig);
// hcan2
hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 12;
hcan2.Init.Mode = CAN_MODE_NORMAL;
hcan2.Init.SyncJumpWidth = CAN_SJW_2TQ;
hcan2.Init.TimeSeg1 = CAN_BS1_11TQ;
hcan2.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan2.Init.TimeTriggeredMode = DISABLE;
hcan2.Init.AutoBusOff = ENABLE;
hcan2.Init.AutoWakeUp = DISABLE;
hcan2.Init.AutoRetransmission = ENABLE;
hcan2.Init.ReceiveFifoLocked = DISABLE;
hcan2.Init.TransmitFifoPriority = DISABLE;
HAL_CAN_Init(&hcan2);
sFilterConfig.FilterIdHigh = (0x183 << 5);
sFilterConfig.FilterIdLow = (0x183 << 5);
sFilterConfig.FilterMaskIdHigh = (0xFFF<< 5);
sFilterConfig.FilterMaskIdLow = (0xFFF << 5);
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO1;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_16BIT;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.FilterBank = 14;
sFilterConfig.SlaveStartFilterBank = 14;
HAL_CAN_ConfigFilter(&hcan2, &sFilterConfig);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.