STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32f4, are bootloader pin specific

In AN2606, it goes into pin specific detail about the pins when look at your specific chip line.   Does this mean that I am limited to those specific pins in order to use the bootloader and that I cannot used an alternate assigned pin?

AndrewC_0-1751918736524.png
Andrew C by Associate III
  • 553 Views
  • 1 replies
  • 1 kudos

FDCAN communication issue with STM32H743ZI Nucleo board

Hi, I am using STM32H743 nucleo board on one of my design. On my board I have installed nucleo board on board to board connector. For FDCAN interface we are using TCAN3414 transceiver IC. Our bit rate is 1MHz and data rate 2MHz for FDCAN communicatio...

DJ_IND_0-1751294920099.png DJ_IND_1-1751294965389.png
DJ_IND by Associate III
  • 2331 Views
  • 10 replies
  • 1 kudos

Resolved! Sending UDP on NetXDuo does not work without breakpoints.

Hi, I have created a program to send UDP using NetXDuo on a Nucleo-H755ZI.I used the URL below as a reference.Creating a dual IPv6 & IPv4 NetXDuo UDP application for STM32H7 using CubeMX  I checked the operation in debug mode and could see that it is...

Hey0256 by Associate II
  • 2776 Views
  • 5 replies
  • 3 kudos

NSS Pin not going high when Idle in SPI

Hi,I am connecting ESP32 with STM32G474RET6 Nucleo board via SPI. I have configured SPI in DMA mode to transfer data. With NSS pin enabled for chip select I can see the pin remains low always during transmission of data and also in idle. So that I co...

BrindhaP by Associate II
  • 1011 Views
  • 3 replies
  • 3 kudos

SPI communication failure at high frequicies

Hi, The SPI communication between an ESP(Master) and the STM(Slave) is failing when i configure the SPI clock at 10MHz.I have STM32F429ZIT6 DISC1 board and i have used SPI3 as slave, the SPI3 is on the APB1 bus which is configured at 45MHz PCLK.The c...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.