2025-03-25 7:39 AM
Hi, I have created a program to send UDP using NetXDuo on a Nucleo-H755ZI.
I used the URL below as a reference.
Creating a dual IPv6 & IPv4 NetXDuo UDP application for STM32H7 using CubeMX
I checked the operation in debug mode and could see that it is sending UDP with Wireshark.
However, when I unchecked “Set breakpoint at:main” in the debug properties and checked without breakpoints, no UDP was sent.
The version of STM32CudeIDE is 1.18.0, X-CUBE-AZRTOS-H7 version is 3.3.0.
How can I send UDP in debug mode without breakpoints or send UDP in RUN mode?
If anyone has a solution, please let me know.
STM32H755ZITX_FLASH.ld could not be uploaded, but the following memory is allocated.
.tcp_sec (NOLOAD) :
{
. = ABSOLUTE(0x24030000);
*(.RxDecripSection)
. = ABSOLUTE(0x24030080);
*(.TxDecripSection)
. = ABSOLUTE(0x24030200);
*(.NetXPoolSection)
} >RAM_D1 AT> FLASH
Solved! Go to Solution.
2025-03-26 5:37 AM
Dear Neil.
Thank you for your reply.
I was surprised to see that the problem is not only a NetDuo problem, but also happens with LWIP.
I also tried updating the Ethernet status with nx_ip_interface_status_check and nx_ip_driver_direct_command, but it did not work.
In the end, adding HAL_Delay(2000) before MX_ThreadXInit() in main.c was a sure thing.
Thanks to your advice, I am now able to send UDP without any problems.
I hope this note of mine will help others.
Thank you again.
2025-03-25 7:42 AM - edited 2025-03-25 7:43 AM
@Hey0256 wrote:when I unchecked “Set breakpoint at:main” in the debug properties and checked without breakpoints, no UDP was sent.
Sounds like there's something you need to wait for at the start of main...
https://community.st.com/t5/stm32-mcus-embedded-software/stm32f767-lwip-tcp-client/m-p/777886
2025-03-26 5:37 AM
Dear Neil.
Thank you for your reply.
I was surprised to see that the problem is not only a NetDuo problem, but also happens with LWIP.
I also tried updating the Ethernet status with nx_ip_interface_status_check and nx_ip_driver_direct_command, but it did not work.
In the end, adding HAL_Delay(2000) before MX_ThreadXInit() in main.c was a sure thing.
Thanks to your advice, I am now able to send UDP without any problems.
I hope this note of mine will help others.
Thank you again.
2025-03-26 5:44 AM
@Hey0256 wrote:I was surprised to see that the problem is not only a NetDuo problem, but also happens with LWIP..
Which certainly suggests that the "problem" is just that something (presumably hardware?) takes a while to "stabilise" - and you just have to wait for that to complete.
What this really needs is someone to look into it and find what, exactly, that thing is - and, thus, how to check for "ready" without just resorting to arbitrary, blind delays.
@ASEHST ?
2025-06-17 9:35 AM
Hello,
This recurring issue has been tracked internally.
An internal ticket (212424) has already been raised for follow-up.
With Regards.
2025-07-07 7:25 AM
Hello,
During the initialization process, the ETH MAC must be configured with the correct Ethernet link speed and duplex mode after the auto-negotiation process is completed, which can take up to a few seconds (see the API HAL_ETH_SetMACConfig).
To resolve the issue, please add the task App_Link_Thread_Entry to your app_netxduo.c file (refer to Nx_TCP_Echo_Client example from X-CUBE-AZRTOS-H7 v3.3.0) .
This task continuously polls the PHY status and updates the MAC configuration if any changes occur to the Ethernet link.
Note: There is no need to add an additional HAL_delay().
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.