STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI data transmission

Using STM32f3xxx series & using SPI2.I wanted to transmit 32 bits data at atime, but in APIHAL_StatusTypeDef HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout) pData is fo r uint8_t.how to transmit uint32?

Bs.1 by Associate II
  • 1501 Views
  • 2 replies
  • 0 kudos

Can not able to transmit continuously

Hi,i am transmit data through can protocol in stm32f103 controller in the while loop and i am doing doing adc and display data on 16x2 lcd so i found that doing this my can transmit is transmitting only 4-5 times amd then stop so i want to ask what c...

ABhat.7 by Associate III
  • 643 Views
  • 0 replies
  • 0 kudos

Timer in Encoder Mode Interrupt via Output Compare

I know, I'm repeating an age old question, but has there been any updates on generating an Interrupt when using a Timer in Encoder mode? I know, that the Interrupt doesn't fire in Encoder mode, but I read in this one thread, that it's somehow possibl...

RKage.2 by Associate II
  • 1809 Views
  • 3 replies
  • 0 kudos

Ordered MCUs have shorted pins

Hello. I recently purchased STM32F405RGT6's. However, out of package and on all of the IC's that I received, I discovered shorts between pins 17 (PA3) and 18 (VSS), which I do not believe should be shorted. I have a few STM32F405RGT6's that I purchas...

LShen.3 by Associate II
  • 2434 Views
  • 7 replies
  • 0 kudos

[SOLVED] --- Encoder very easy code ---

Here the code to read encoder.unsigned int Enc_dir; unsigned int save_a = 0, save_b = 0;       void BSP_Encoder_Init() { GPIO_InitTypeDef gpio_init_structure;   __HAL_RCC_GPIOF_CLK_ENABLE();   gpio_init_structure.Pin = GPIO_PIN_8; gpio_in...

STM32F746 Flash Memory Organization?

The datasheet for the STM32F746VET shows that it has 512k bytes of Flash. But the Reference Manual for the STM32F74xxx shows 1Mbyte of Flash (sectors 0 thru 7). Do we just assume that sectors 6 and 7 don't exist? This seems a bit vague.

0693W000008y5wvQAA.png

Resolved! STM32L476 SPI NSS bit not functioning

Using an stm32l476rg nucleo as a master device and SPI2 peripheral. The following bits have been set in order for the NSS bit to stay high normally and then be pulled down during communication (according to the reference manual).MSTR = 1SSM = 0SSOE =...

ZHama.1 by Associate II
  • 1586 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.