2021-03-27 10:15 AM
I know, I'm repeating an age old question, but has there been any updates on generating an Interrupt when using a Timer in Encoder mode? I know, that the Interrupt doesn't fire in Encoder mode, but I read in this one thread, that it's somehow possible to set Channel 3 and 4 to Output Compare no Output and somehow create an interrupt that way, but that was a bit confusing. Can any one help?
2021-03-27 10:41 AM
> generating an Interrupt when using a Timer in Encoder mode
Interrupt upon what? What do you want to achieve? What exactly is confusing in the linked thread?
JW
2021-03-27 11:21 AM
Interrupt on the encoder value changing.
The linked thread is confusion because I tried it, but simply nothing happens.
This a classic case of something beeing pretty simple, if you know how it works, but seems impossible, when you don't.
SMT32 Timers can be pretty confusing, even though I have read the Application Notes and the reference manual.
2021-03-27 3:11 PM
> The linked thread is confusion because I tried it, but simply nothing happens.
What exactly did you try, and what "nothing happens" exactly means?
> Interrupt on the encoder value changing.
I'm not sure why this would be useful.
The linked thread discusses something different: interrupt upon reaching a predetermined value.
Value is changing when an edge arrives on one or both channels CH1/CH2 (depending on the particular encoder mode selected), so you simply set up an input capture interrupt on the given channel.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.