2021-03-27 11:14 AM
Here the code to read encoder.
unsigned int Enc_dir;
unsigned int save_a = 0, save_b = 0;
void BSP_Encoder_Init()
{
GPIO_InitTypeDef gpio_init_structure;
__HAL_RCC_GPIOF_CLK_ENABLE();
gpio_init_structure.Pin = GPIO_PIN_8;
gpio_init_structure.Mode = GPIO_MODE_IT_RISING_FALLING;
gpio_init_structure.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOF, &gpio_init_structure);
gpio_init_structure.Pin = GPIO_PIN_9;
gpio_init_structure.Mode = GPIO_MODE_IT_RISING_FALLING;
gpio_init_structure.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOF, &gpio_init_structure);
HAL_NVIC_SetPriority(EXTI9_5_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);
}
void EXTI9_5_IRQHandler(void)
{
uint8_t now_a;
uint8_t now_b;
now_a = HAL_GPIO_ReadPin(GPIOF, GPIO_PIN_8);
now_b = HAL_GPIO_ReadPin(GPIOF, GPIO_PIN_9);
if (!save_a & !save_b)
{
if (now_a)
{
save_a = now_a;
Enc_dir = 2;
}
if (now_b)
{
save_b = now_b;
Enc_dir = 1;
}
}
if (save_a & !save_b)
{
if (!now_a)
{
save_a = now_a;
Enc_dir = 1;
}
if (now_b && now_a)
{
save_b = now_b;
Enc_dir = 2;
}
}
if (save_a & save_b)
{
if (!now_a)
{
save_a = now_a;
Enc_dir = 2;
}
if (!now_b)
{
save_b = now_b;
Enc_dir = 1;
}
}
if ((!save_a) & (save_b))
{
if (now_a)
{
save_a = now_a;
Enc_dir = 1;
}
if (!now_b)
{
save_b = now_b;
Enc_dir = 2;
}
}
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_8);
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_9);
}
......
if (Enc_dir > 0)
{
if (Enc_dir == 2)
buttonUpClicked();
else
buttonDownClicked();
Enc_dir = 0;
}
2021-03-27 3:03 PM
I personally would run this in regular timer interrupt, unless your encoder is a "machine" one with guaranteed no bouncing on edges (i.e. not the hand-turned input).
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.