STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Compatible MCU among stm32f4 series

Hi, everyone. I am Emily.​ I would like to know the MCU which is compatible to 'stm32f446RET'.​Also I wanna double-check the possiblity of compatible usage between 'stm32f407VET'​ and 'stm32f417VET'.​Please help me:crying_face:​

EHa.1 by Associate II
  • 2565 Views
  • 3 replies
  • 0 kudos

[X-cube-AI] Does stm32 F/H arm coretex-M7 series hardware has TPU(tensor processing unit) for hardware accelation ?

Hello. I want to know does stm32 cortex m7 series has TPU (tensor processing unit) for hardware acceleration. I heard that TPU has a systolic array which is a network of processors that are responsible for performing computations and passing the resu...

0693W000008ywRRQAY.jpg
Yjang.1 by Associate II
  • 3822 Views
  • 4 replies
  • 0 kudos

Resolved! ADC Sampling of Voltages > 2.8V effects VDD

Using STM32L431RCT6 (VDDA and VREF+ bondet together). VDDA/VREF is 3.0V and VDD is 1.8V. If i'm sampling voltages larger then 2.8V that effects VDD (Jumping from 1.8V to approx. 2.06V for approx. 400ms). Any Idea's what i'm doing wrong?

MGehr.3 by Associate II
  • 2157 Views
  • 4 replies
  • 1 kudos

I want know ADC setting is correct.

I have just received the code from my predecessor. The company said something garbage value in ADC sometime.I think is must be ADC problem. ​I don't know what is wrong where cause it. Setting is wrong?I use STM32F103RCT6 MCU.I checked that ADC uses a...

zzzjizon by Associate
  • 955 Views
  • 0 replies
  • 0 kudos

Switching a code base from stm32l010RB to stm32L010K4

Hi,I am currently trying to switch my code base from the RB version of the L010 family to the K4 version. I am doing this because the dev board I prototyped on was for the RB variant. I am building with arm (Keil).I am running into some issues in thi...

rsoc by Associate III
  • 1097 Views
  • 1 replies
  • 0 kudos

Resolved! How to port a project from a STM32L476RG to a STM32L072CZYx

Hello,I'm working on a BLE project on a STM32L072CZYx MCU and there is an example of a profile that suits my need but it is on another MCU, the STM32L476RG. I want to port the code from that MCU to mine but I don't really know how to do so... I've ch...

MBour.2 by Associate II
  • 1876 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.