STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I use external SPI flash memory as a heap

Hello @All ALL​ ,@Martin KJELDSEN​ ,I am using STM32F412CGU6 Microcontroller.I would like to use external SPI flash memory as heap.Can you please give me some idea?Can you please suggest me the required changes in linker script?Is there any document ...

Resolved! Out-of-spec temperature behavior of STM32F412 (hard fault) ?

Hi all,I am testing product samples fitted with STM32F412RET6 which has a temperature operating range of -40°C +85°C.On some samples tested inside a climate chamber, the MCU unexpectedly reset due to cold temperature within operating range (e.g. -5°C...

MLiis.1 by Associate II
  • 3736 Views
  • 6 replies
  • 0 kudos

Log numeric data in SWV ITM Data Console

Is it possible to customize the display format of ITM data in the "SWV ITM Data Console" view to show the raw data values, rather than the text interpretation?For example, I'm writing various counter values to different ITM ports, and would like a co...

0693W000007EEUpQAO.png 0693W000007EEUuQAO.png
Miles1 by Associate III
  • 1812 Views
  • 1 replies
  • 3 kudos

Timer Input randomly skips interrupt.

I'm sertanly missing something.I have a board with STM32F103 that control fan via PWM and have to check it's speed with Fan's TACH out. TACH out is consistent PWM signal with duty cicle 50% and frequency 80 Hz.Chip is running with 64MHz clock, APB1 i...

0693W000008yz12QAA.png
viteo by Associate II
  • 4089 Views
  • 7 replies
  • 0 kudos

STM32H745 Nucleo: ADC with DMA don't work

Hi! I have STM32H745 Nucleo and i want to transfer data from ADC via DMA.1. At first i write code for ADC with out DMA (ADC3, PF10 in) and it work excellent. I get positive knovlege.2. At second step i tried to use DMA (DMA1 stream 1), but code don't...

AAnt.1 by Associate II
  • 2104 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.