2021-04-08 5:41 PM
I have just received the code from my predecessor.
The company said something garbage value in ADC sometime.
I think is must be ADC problem.
I don't know what is wrong where cause it. Setting is wrong?
I use STM32F103RCT6 MCU.
I checked that ADC uses a single ADC and multiple channels.
I write here init code and ADC code.
void ADC_Initial(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
/* Enable ADC1 and GPIOC clock */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC, ENABLE);
// GPIOC
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOC, &GPIO_InitStructure);
// GPIOB
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* ADC1 configuration ------------------------------------------------------*/
ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; //independent v dual
ADC_InitStructure.ADC_ScanConvMode = DISABLE; //multiChannel SingleChannel v
ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;//ENABLE; //not continuous Mode
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfChannel = ADC_CH_MAX+1;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel 9~15 configuration */
ADC_RegularChannelConfig(ADC1, ADC_Channel_9 | ADC_Channel_10|ADC_Channel_11|ADC_Channel_12|ADC_Channel_13|ADC_Channel_14|ADC_Channel_15, 1, ADC_SampleTime_13Cycles5); //
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
/* Enable ADC1 reset calibaration register */
ADC_ResetCalibration(ADC1);
/* Check the end of ADC1 reset calibration register */
while(ADC_GetResetCalibrationStatus(ADC1));
/* Start ADC1 calibaration */
ADC_StartCalibration(ADC1);
/* Check the end of ADC1 calibration */
while(ADC_GetCalibrationStatus(ADC1));
/* Start ADC1 Software Conversion */
ADC_SoftwareStartConvCmd(ADC1, ENABLE);
ADC_BufferClear();//this is our code.
}
void ADC_ReadData(void)
{
int i;
for(i=0;i<ADC_CH_MAX;i++)
{
if(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET)
{
/// 만약�? ADC Enable�?� 안�?�어 있으면.
ADC_RegularChannelConfig(ADC1, ADC_CH_BASE + i, 1, ADC_SampleTime_55Cycles5);
ADC_Cmd(ADC1, ENABLE); //enable ADC1
while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET);
}
ADC_Buffer[i][ADC_BufferIndex] = ADC_GetConversionValue(ADC1);
}
ADC_BufferIndex++;
if(ADC_BufferIndex >= ADC_SAMPLE_MAX)
ADC_BufferIndex = 0;
// Avg
ADC_Average();
}
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.