2021-04-06 7:14 AM
Hello,
I am trying to use a 240x320 ili9341 screen with g030 but even one picture doens't fit into flash memory. (If you are familiar with ILI9341, the picture I am talking about is snow_tiger)
I made some research on it and saw that in TouchGFX website STM32G071 nucleo board with the X-Nucleo-GFX01M1 expansion board is used. The expansion board has 64-Mbit SPI NOR Flash memory.
If I buy a NOR Flash memory, can I overcome my problem?
Thank you
2021-04-06 7:26 AM
I tried using SD Card but when I imported FATFS middeware on CubeMX, RAM overflowed :(
2021-04-06 8:44 AM
It doesn't provide for a QSPI interface, so can't be mapped into the processors memory space, or allow for Execute-In-Place.
SPI access should be viable, and have a relatively small code foot-print.
You could page data and code into RAM.
2021-04-06 11:41 AM
You can add SPI memory, but with 8kB RAM i mean you waste time with 030 try work with graphics. Why not start with other?
2021-04-09 12:03 AM
Okay guys thank you for the answers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.