STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Can someone advice a psram for STM32F479 LQFP100 ?

Dear Community,can someone advice a min 8Mbit psram for the STM32F479?I only find some who has address pins up to A20 but the uc has only up to 16 or did I missunterstand something?best regards

Dany1 by Associate
  • 2849 Views
  • 3 replies
  • 0 kudos

I can't work SPI Transmit with DMA by LL Library

Hi Seniors.I am a beginner who started to implement in the LL library.I would appreciate it if you could help me.What I want to do is very simple, I want to transfer one buffer divided into front and back by SPI (Slave) using DMA every second.The imp...

HNish.1 by Associate
  • 852 Views
  • 0 replies
  • 0 kudos

I am looking for working without hardware failure, testing report and status of obsolescence for 10 years and certification data.

Good Morning Sir,I am looking for working without hardware failure, testing report and status of obsolescence for 10 years and certification data. Part no of following component are:497-STM32L476ZGT6CT-ND497-BLUENRG-M2SPCT-NDSTC3100ISTM24M02-DRMN6TP4...

RJat by Associate
  • 825 Views
  • 0 replies
  • 0 kudos

STM32F469 SPI DMA repeat TX while filling RX buffer?

Hi thereI got an IC that needs to be fed with 32bit NOP words via SPI TX (0x00000000) to get 32bit data output via RX at the same time. Communication works fine in SPI polling mode but I really want to try to do it via DMA...My RX buffer is an array ...

0693W000008zC2SQAU.png
PGroe.2 by Associate III
  • 1846 Views
  • 2 replies
  • 0 kudos

HAL_Delay stuck in Loop

Hello!First of all, im pretty new to programming STMs. I'm currently working on a project on the WL Series and stuck with the HAL_Delay function. Even something super simple like toggling my User LED won't work.For RCC im using a TCXO 32Mhz as HSE.wh...

0693W000008ys3zQAA.png 0693W000008ys5MQAQ.png
GHube.1 by Associate II
  • 8291 Views
  • 6 replies
  • 1 kudos

Use of an external SDRAM (IS42S16320F) with STM32H753

Hello!I'm trying to use an external SDRAM (IS42S16320F) with an STM32H753 but no luck till now.Could please anyone check if my settings are correct because I don't know if I made a bug here.  For that I have attached the FMC configuration and the sch...

0693W000008yud1QAA.png 0693W000008yudBQAQ.png 0693W000008yudGQAQ.png
Gregory3 by Associate III
  • 7727 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.