STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

A qutetion about STM32F429 IAP program

Hi ! there is a question about my program: I use a bigger array ,size is 10K , in my app program ,my IAP bootloader program can jump to app program ,and it works. but when I change it up to 20K , app doesn't work.And the app works even array's siz...

Hhh.1 by Associate
  • 719 Views
  • 0 replies
  • 0 kudos

Stm32f730i8 spi issue

Hi, I am using stm32f730i8 chip set for my application, whereas I am communicating the peripheral through spi where I need high frequency clock. But currently I am able to operate with 2MHz if I increase beyond that the spi clock is getting skewed.Pl...

KSiva.11 by Associate
  • 1086 Views
  • 1 replies
  • 0 kudos

Clearing the SPI Buffer

Hi all, I'm working on a project where I am using an STM32F3 (master) to communicate with an STM32G0 (slave) using SPI with DMA. The G0 performs a task and can receive commands, and have it's "registers" (ie. state data) read out over the SPI. I want...

Konami by Senior II
  • 985 Views
  • 0 replies
  • 0 kudos

How to change MSI frequency on the fly ?

Hi, I am working on an STM32L476RCT6 and I use STM32CubeMX to configure the peripherals of the microcontroller.Currently the microcontroller runs on MSI, whose frequency is set at 8 MHz. The clock configuration is as follows :I want to use the USB in...

0693W000008zHvSQAU.png 0693W000008zHsAQAU.png
VGava by Associate II
  • 2617 Views
  • 3 replies
  • 0 kudos

STM32H735-DK reset

I have a demoboard STM32H735-DK. I develop a demo for my customer. All OK. But when I supply the card (with USB cable) the application-firmware doesn't run: I have to press the button reset for start it. Why? Thanks for your answer.

MGatt.2 by Associate II
  • 1021 Views
  • 1 replies
  • 0 kudos

NUCLEO-L412RB Pin stopped working as input

Im not sure if i fried a pin or if i am missing something, but i a using a NUCLEO-L412RBhttps://www.st.com/resource/en/user_manual/dm00387966-stm32-nucleo-64-p-boards-stmicroelectronics.pdfand i can use in PA6 as an ouput pin fine, but for some reaso...

TShem.1 by Associate II
  • 2860 Views
  • 6 replies
  • 0 kudos

Wake up pin identify issue

I use 3 wake up pin PA0,PC5 and PC13 .(MCU part number is STM32L452)When trigger wake up pin to wake up MCU from the standby mode.How to identify which WAKE UP PIN is triggered?

Adams by Associate II
  • 1604 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.