STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 USART1 DMA is not working..

Hi team,I'm using STM32H753BI. Here i'm using USART1 (PA9 & PA10) in DMA Mode. That code is generated by cubeMX and also i tried the example program of STM32H743-EVAL Board. Both are not working.Here i have attached the hal_msp_file.c and main.c for...

Vel by Associate III
  • 9740 Views
  • 12 replies
  • 0 kudos

What's current manfucaturing situation with STM32?

Dear ST, as manufacturer we are facing issue with part availability for :STM32F030RCT. We are trying to find alternative part however stock level for every single MPU that i have found is 0. Could You please provide details about LT in EU?

JDomi.2 by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

Not initialized RAM segment on STM32H7 dualcore

I successfully create 0x40 bytes on "not initialized" area on top of AXI RAM (0x24000000) for CORE M7 and on top of AHB SRAM1 (0x30000000) in order to info about a fault immediately before reset MCU (for example if a trap of NULL pointer is triggered...

Resolved! How to come out from sleep mode using CAN interrupt?

Hello All, I am using sleep mode to save power. I am using STM32L431RC & using CAN interface.I am able to enter into the sleep mode when a CAN message is received. But it doesn't come out when a CAN interrupt is received.My code for CAN interrupt han...

J75888.1 by Associate II
  • 1742 Views
  • 2 replies
  • 0 kudos

Resolved! Why pinrst is configured after sftrst

If you run it with the reset pin, you can use the "__HAL_RCC_GET_FLAG()" functionYou can see that "RCC_FLAG_PINRST" is set.However, when executed with "HAL_NVIC_SystemReset()", "RCC_FLAG_SFTRST" and "RCC_FLAG_PINRST" are set.My expectation is that on...

ckim.2390 by Associate II
  • 3084 Views
  • 3 replies
  • 1 kudos

Help debugging HardFault on STM32F446 using STM32CubeIDE

I have an application running on an ST32F446 using code generated by STM32CubeMX. I use SPI1 in slave mode to receive commands, and have FATFS operating with USB HOST to connect to a USB FLASH drive. I can send commands via the SPI interface to open ...

krubow by Associate II
  • 2481 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.