STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Only single ADC in F401 and F411

This is not a question, more like a statement and proposal to update datasheet.In these two datasheet:DS9716, STM32F401xB STM32F401xC, DS9716 Rev 11, page 105/139DS10314, STM32F411xC STM32F411xE, DocID026289 Rev 7, page 114/149It are specified sample...

Problem with two simmilar projects

Greetings everyone!Lately, I have generated two projects for Nucleo-STM32H745ZI EvB.The first one was generated just for the MCU and for the second one I have chosen the EvB as a reference. So now I do have two quite simmilar projects where the first...

APlot.1 by Associate II
  • 1876 Views
  • 4 replies
  • 0 kudos

STM32H7 Huge program with UART Tx using DMA

Hey guys!This probably came up 5000 times, however I did try to look for a solution before I ask this one. Couldn't find one.I am having issues transmitting data via uart with DMA.Problem:The problems I am having is that the RxBuffer is not receiving...

CLeo.1 by Senior II
  • 3499 Views
  • 1 replies
  • 0 kudos

I am interfacing TFmini S LIDAR with nucleo STM32F103, I am using 2 UARTS, uart1 and uart3 to receive LIDAR data. I am using DMA for that. LIDAR frequency is 1000Hz and data length is 9 bytes. uart 1 and 3 baudrate is set to 256000.

I am using HAL_UART_ErrorCallback() function to capture any error.When I reset the the board by cutting the power off everything works fine. But if I reset it with reset button or software reset one of the uart freezes and I don't see any error. I ha...

PKand.2 by Associate II
  • 2903 Views
  • 6 replies
  • 0 kudos

How to write non-reserved option bytes on STM32H750xx MCU?

Hello!The STM32H750xx data sheet states that the MCU has 2KB of space in flash memory for "option bytes." However, the programming reference describes on page 176 that "Table 21 lists all the user option bytes managed through the embedded Flash memor...

briankaz by Associate III
  • 2482 Views
  • 2 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.