STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt mapping to NVIC ISR vector

I was looking at the ARM M7 reference manual, and it shows an empty NVIC ISR vector from 0x40 to 0x3fc. When I look at the file startup_stm32h725xx.s it defines specific interrupts mapped to the ISR vector. Are these hard mapped by the EXTI block an...

DCons.1 by Associate
  • 2658 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H7 Hard Fault when RCC at 165 MHz

I have the STM32H7B3I-DK (MCU: STM32H7B3LIH6Q), and I am trying to get the sys_ck close to its maximum frequency of 280 MHz, by running HSI or HSE through PLL. The trouble is that I can only get up to 164 MHz. Any higher and I get a hard fault. Is th...

FSkro.1 by Associate II
  • 1379 Views
  • 1 replies
  • 0 kudos

STM32F767 ZI, Trouble understanding how HAL_I2C_MASTER transmit works. Trying to send 32 bit adc data over I2C

So I am trying to send an ADC value that I receiving on the board over I2C to another device. I have adc_Value as a 32 bit one since the ADC read function on HAL is 32 bits. I want to send this over i2c. Currently I have this.  HAL_ADC_Start(&hadc1);...

HSyed.1 by Associate II
  • 2426 Views
  • 4 replies
  • 0 kudos

Resolved! How to use DMA on complementary timer channels in TIM1

I have been trying to start PWM on TIM1 with complementary channels and use DMA to start the PWM. The problem that I have is that only one of the channels will start when I run the program. DMA channel 2 is being used by TIM1_CH1 and I can't find any...

Mhass.12 by Associate II
  • 4373 Views
  • 4 replies
  • 0 kudos

HAL_Delay stuck when sdram use as data memory

Hi:I have a custom STM32F746NG board with SDRAM IS42S328200D(Address 11 bits 2^11(Row Address)*2^8(Column Address)*32(bit)*4(bank)). My goal is to use sdram as data memory, I followed example in STM32Cube_FW_F7_V1.16.1\Projects\STM32746G-Discovery\Ex...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.