2021-06-26 8:00 PM
Hi:
I have a custom STM32F746NG board with SDRAM IS42S328200D(Address 11 bits 2^11(Row Address)*2^8(Column Address)*32(bit)*4(bank)).
My goal is to use sdram as data memory, I followed example in STM32Cube_FW_F7_V1.16.1\Projects\STM32746G-Discovery\Examples\FMC\FMC_SDRAM_DataMemory.
1.modified STM32F746NGHx_FLASH.ld
2.modified startup_stm32f746xx.s
3.modidied system_stm32f7xx.c
4.initialize uart1 to print log and light a led.
But the HAL_Delay is stuck, and it is strange, sometimes HAL_Delay won't be stuck, but if I rebuild project, it will be stuck.
meanwhile, I noticed when it is stuck, I move bl SystemInit(in startup_stm32f746xx.s) to another line(from line 65 to line 96), it won't be stuck.
I think the reason should be systick interrupter not be called and memory map is related to this, but I don't know why.
I also add -mno-unaligned-access when build project, but nothing change.
I attached my project example. It included all file I modified.
2021-06-26 8:46 PM
> stuck,... struct, ... struck.
What does stuck/struct/struck mean? When you debug the code, where is it?
Note that SysTick needs to be higher priority that the current interrupt you're in since HAL_Delay relies on it being called.
I would look at your SDRAM timings to ensure they are consistent with the timings in the datasheet. Could be getting a hard fault here.
2021-06-27 6:21 AM
stuck means freeze, doesn't it?the other two words are misspelled, I have corrected them.
when code run to Hal_Delay, it will loop in Hal_Delay function. of course I debug the code, that is why I said Hal_Delay cause my problem.
I have set systick priority to 0, so the reason is not this.
the sdram timing should be ok, because the data I write to sdram is same as I read when I use internal ram as data memory.
2021-06-27 7:12 AM
So it's executing a loop within HAL_Delay and never returning? I don't see why SysTick would suddenly stop executing, unless there's a hard fault you're missing. The HAL_Delay code is simple, surely that's not the issue.
2021-06-28 4:10 AM
I debug the code, hard fault didn't trigger, when I remove Hal_delay, the uart print function works fine. the log output from uart1.
I think memory map may be wrong, but I have no ideal about this
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.