STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Replace RTC Crystal with RTC Oscillator ?

We are working on a custom board based on STM32L476RGT6, and we are facing 32.768Khz crystal startup issue. Board stucks at the startup in following piece of code : HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) and it fails while waiting for RCC_L...

MAhme.4 by Associate II
  • 1793 Views
  • 1 replies
  • 0 kudos

Having problem with UART communication in Interrupt mode

I am doing a project on STM32H747 DISCO Discovery board involving UART. I am sending one string continuoulsy with 5 seconds delay from esp32 to stm32. I am able to receive the string in polling mode but I am not able to receive the string in Interrup...

SLuit.1 by Associate III
  • 1150 Views
  • 2 replies
  • 0 kudos

Weird PWM Timer3 master and PWM Timer1 slave behaviour

Hello, I have a timer 3 master and timer 1 slave. When a button is pressed, master is activated as long as button is pressed, and then slave is triggered based on master's output signal (high / low) (gated slave control)(This is a continuation of my...

0693W00000BcAQEQA3.png 0693W00000BcAQiQAN.png 0693W00000BcAHIQA3.png 0693W00000BcAO4QAN.png
Xxoyo.1 by Associate III
  • 2217 Views
  • 4 replies
  • 0 kudos

STM32F746GDISCOVERY, PWR_PVD, STM32CubeIDE

I want to make an interrupt when power > 2.0V. STM32CubeIDE generated:/** * @brief NVIC Configuration. * @retval None */ static void MX_NVIC_Init(void) { /* PVD_IRQn interrupt configuration */ HAL_NVIC_SetPriority(PVD_IRQn, 8, 0); HAL_NVI...

Resolved! RTC inaccuracy induced by internal clock source?

I'm using the STM32L431xx mcu. The current hardware configuration of our design has no external clock source (crystal), so we are using the internal one. And there's a new functionality which demands second-accurate real time clock, over a period of...

I2C in DMA mode - deadlock on I2C interrupt

Has anyone have similiar issues ? I got I2C DMA writes working nicely on table, but in real application there are disturbances which cause false start condition on the bus.This happen when I2C HAL driver has "lock" on I2C handle - so incoming interr...

Forcing Capture-Compare-Register to clear [STM32H7]

I'm trying to count the number transition during the time another process is taking place. Don't need frequency, just the counts.So I've enabled TIM8CH3 for capture-compare, and have verified that CCR3 does change when there are transitions on th...

bnguy.1 by Associate III
  • 4801 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.