2021-06-24 3:26 AM
Hey,
I found an error in the STM32F410 Reference Manual (RM0401 Rev 3). I'm not exactly sure, if this is the right place to highlight errors in the datasheet, but maybe an employee of ST can verify the error and eventually forward it to the person which can correct it in the manual.
Link to the Reference Manual RM0401 Rev 3:
In section "3.3 Embedded Flash memory" on page 46, there is the "Table 5. Flash module organization", which says that the block base addresses of sector 4 starts at 0x08011000 but it actually starts at 0x08010000
I verified it, by writing data to the flash and then erased sector 4 -> The erased part starts at address 0x08010000
Thanks and best regards
Julian
Solved! Go to Solution.
2021-06-28 6:10 AM
Hi @Julian Wörle ,
You are right, it is a typo. Sector 4 start at 0x08010000.
I raised this error internally for correction in the coming releases of the RM0401.
Thanks again for noticing us.
Imen
2021-06-24 4:05 AM
Hello @Julian Wörle and thanks for posting this issue.
I will check this internally and come back to you with update.
Imen
2021-06-28 6:10 AM
Hi @Julian Wörle ,
You are right, it is a typo. Sector 4 start at 0x08010000.
I raised this error internally for correction in the coming releases of the RM0401.
Thanks again for noticing us.
Imen
2021-06-28 6:38 AM
Thanks @Imen DAHMEN for the quick verification
Best regards
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.