STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Power domains on STM32L552ZET6

Hi guys,I have a short question regarding the STM32L552ZET6 power domaines. Can I use 1v8 to power the chip and connect a 3v3 power supply on the VDDIO2 which I will power on from time to time(when I need to use those pins)? And another thing if I do...

CDan.1 by Associate II
  • 1461 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F4: 4-bits SDIO DMA - Data Corruption in SD card

Hi, I'm currently using STM32F401RE Nucleo-64 Board. My current objective is to store all the data collected from ISM330DLC Accelerometer, into SD card through SDIO protocol.BackgroundMost of the setup is based on Code generation, using STM32CubeIDE ...

ZTan.2 by Associate II
  • 7485 Views
  • 6 replies
  • 1 kudos

Resolved! Is it Possible to change the timer count direction dynamically without having to wait for it to over- or underflow?

Hello dear ST-Community,here is a brief explaination of my problem:I'm using multiple stepper-motors in my system.I want to use 3 timers per stepper.Timer generates the PWM signal for the stepper-driver (easy to achive)Timer captures the signal of th...

JHöfl.1 by Associate III
  • 2842 Views
  • 3 replies
  • 0 kudos

How to decode LVDS data

I've a camera using lvds protocol, now using LVDS to LVTTL converter connect to stm32f730r8t6.​I want to decode lvds data and fifo it to USB.​But first problem is could stm32 decode 20Mhz lvttl clock?I've tried to use tim input captuer clock and usin...

0693W00000D1ii6QAB.png 0693W00000D1iiuQAB.png 0693W00000D1ijYQAR.png
HL.2 by Associate II
  • 3913 Views
  • 4 replies
  • 0 kudos

My F3Discovery board is not recognised.

On my f3 discovery board, i was measuring voltage between 5v pin and GND with multi meter and the power LED started blinking . When i removed the the multimeter i noticed the com LED is turned off and the board disappeared from ports in device manage...

0693W00000D23IdQAJ.png
asim khan by Associate III
  • 1632 Views
  • 2 replies
  • 0 kudos

RM0440, Rev 6, STM32G4 Reference Manual - Errors

Figure 151, Page 682: The second line in the picture should be "ADC Master EOC".Section 27.5.68, Page 1054: Description for bit 20 ADCTBRST should be similar to bit 14. Currently, it is a circular reference to itself "Refer to ADC3TBRST description."...

How to disable JTAG on STM32H743XIH6?

Hello there, we're using STM32H743XIH6 MCU for out development.We're at a stage where, we need JTAG to be disabled for Production build and enabled for the Debug build.In order to do that, I searched online, and figured that RDP level can be set to d...

JJ1 by Associate II
  • 4296 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.