2021-08-10 3:55 AM
Hello dear ST-Community,
here is a brief explaination of my problem:
I'm using multiple stepper-motors in my system.
I want to use 3 timers per stepper.
My Problem is, that I need to change the conting direction of the 3. Timer according to the rotational direction of the motor. I change direction of the motor in software, so all I thougt I needed to do was to change the count-direction of the 3. Timer simultaniously.
Is this possible? I coundn't find a __HAL-Macro for chainging the timers counting direction at runtime. I know it corresponds to the timers CR1 register, but woudn't it wait for the timer to over- or underflow until the change takes effect? Sadly I can't confirm it with hardware atm because I'm still waiting for my drivers.
My last resort would be to store the timers value befor chainging direction and resetting it with a new arr. So if I'm changing from a up-couting mode to down-counting, I'd have to store the CNT, reset the timer, change direction and use the stored CNT as new ARR. Then the down-counting would start from that ARR.
The whole reason for using 3 timers for one motor is to minimize cpu time, so I'd like to just change a register when I change direction and nothing more.
I'd love to here from an experienced timer-user if this approch is an good or if there is something more elegant.
Thanks in andvance!
Greetings from Germany
johofz
Solved! Go to Solution.
2021-08-10 4:48 AM
I'm not trying to understand and critique your particular application/approach.
> I coundn't find a __HAL-Macro for chainging the timers counting direction at runtime.
Cube/HAL is a "library" which inevitably implements only a fraction of what's possible with the hardware. It's main purpose is to support the clicky CubeMX. There's no reason to seek constraints in Cube/HAL; read the TIM chapter in RM and proceed accordingly.
> I know it corresponds to the timers CR1 register, but woudn't it wait for the timer to over- or underflow until the change takes effect?
No. Just read the description of the TIMx_CR1.DIR bit.
> Sadly I can't confirm it with hardware atm because I'm still waiting for my drivers.
You surely can play with the timer itself on any cheap Nucleo board. Do it, it's fun.
JW
2021-08-10 4:48 AM
I'm not trying to understand and critique your particular application/approach.
> I coundn't find a __HAL-Macro for chainging the timers counting direction at runtime.
Cube/HAL is a "library" which inevitably implements only a fraction of what's possible with the hardware. It's main purpose is to support the clicky CubeMX. There's no reason to seek constraints in Cube/HAL; read the TIM chapter in RM and proceed accordingly.
> I know it corresponds to the timers CR1 register, but woudn't it wait for the timer to over- or underflow until the change takes effect?
No. Just read the description of the TIMx_CR1.DIR bit.
> Sadly I can't confirm it with hardware atm because I'm still waiting for my drivers.
You surely can play with the timer itself on any cheap Nucleo board. Do it, it's fun.
JW
2021-08-10 5:59 AM
You can use LL_TIM_SetCounterMode(TIMx, LL_TIM_COUNTERMODE_UP) to do this.
Modifying registers directly seems smarter here.
2021-08-10 10:37 AM
Thanks for the answers!
It worked with just modifying the DIR bit like so:
m_positionTimer->Instance->CR1 |= TIM_CR1_DIR;
and
m_positionTimer->Instance->CR1 &= ~(TIM_CR1_DIR);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.