STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use two DAC channels simultaneously

Hello,I am using STM32F765BI MCU. As per our requirement we have to send data on both the DAC channels simultaneously using DMA. but I could not find any API for this. There are APIs available for DAC DMA single channel only as shown below,HAL_Statu...

LDesa.1 by Associate II
  • 4772 Views
  • 3 replies
  • 0 kudos

Resolved! [SOLVED] Nucleo STM32l4R5ZI Vref Buffer stuck on Timeout

Hello,I am trying to output the reference voltage for the DAC in a Nucleo L4R5ZI, I am doing so with the Vref Buffer. I am using STM32CubeIDE.After creating a default project I just disabled all the communication I wasn't going to need and I configur...

DMart.16 by Associate II
  • 2252 Views
  • 3 replies
  • 0 kudos

Issues with UART1 on STM32F303RT8

Hi I am working on getting and processing raw serial data on a STM32F303RT8 MCU. The interrupt is firing but I am not able to properly read data from the Serial interface.Every time the ISR fires, the value of "sr" is 216 except for the first time w...

PVD IT always rising

I'm working on a STM32L072, and I tried to configure the PVD to rising an IT when the supply voltage is below 2.7V.It appears that the IT is always rise even the voltage is always above 3V. __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_...

Ppeyr.1 by Associate III
  • 1767 Views
  • 4 replies
  • 0 kudos

GPIO UART disable and enable

Hi I use UART very rarely and I would like to disable gpio:void Disable_Not_Used_Pins(void) { /* Disable UART pins*/ GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GP...

ughr1 by Associate II
  • 1388 Views
  • 2 replies
  • 0 kudos

Resolved! Debug issue

Hello,I am using ST-LINK/V2 (STM32 Nucleo-64) to debug a custom board, which the custom board use STM32F105VC MCU.The HW connections are as follow: SWD, Custom Board3.3V, 3.3VSWCLK, PA14GND, GNDSWDIO, PA13NRST, PB4 (NJTRST)SWO, Not useMaybe E1 (NRST)...

NASI by Senior
  • 4844 Views
  • 8 replies
  • 0 kudos

Hello guys. before all, I appreciated your Hint and Help. I use STM32L4R9Z microcontroller to Drive a QuadSPI NAND-Flash(Winbond). I configured OctaSPI of microcontroller as QuadSPI, and tried to write on NAND-Flash at Auto Polling mode.

After the Write-Enable command has been executed, the "HAL_OSPI_AutoPolling()" function will be called but, at the line of :status = OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_SM, SET, tickstart, Timeout);time out event will be accrued and s...

HBita.1 by Associate
  • 4417 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.