2021-08-10 2:06 AM
Is there any available example or threads for using multiple SPI slaves on the single SPI bus?
2021-08-10 6:07 AM
Which chip?
Multiple slaves is conceptually quite similar to a single slave. Use a different CS pin for each slave and toggle them as you want to talk to each chip.
2021-08-10 6:32 AM
Thanks for replying.
I have STM32L496ZG.
I am specifically looking for SPI flash as one of the SPI slaves in multiple SLAVE scenarios on the single SPI bus.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.