STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743 (I/O direction control of SDMMC CMD signal)

I'm thinking of getting STM32H743 to work Wi-Fi module via uSD.However since I can not get my Wi-Fi module responding I start questioning my design.​SDMMC POWER.DIPOL control but can change the polarity of CIDR, D0DIR, D123DIR,Is there a way to chang...

MSugi.1 by Associate II
  • 2614 Views
  • 6 replies
  • 0 kudos

STM32F7 resetting during flash operation

I have a project that was working at one point but is no longer working. I think I've narrowed the issue down to a couple of flash operations that happen during setup for Azure IOT. If I let the system run normally it will keep resetting and not run....

EReye.2 by Associate
  • 2125 Views
  • 4 replies
  • 0 kudos

stm32f7 as spi slave

Hi. I am trying to work with AD7763. I have the same problem as in this article, but there are no answers in it. https://community.st.com/s/question/0D50X00009Xkfaw/spi-oneway-communication-slavemaster?t=1639997683527So AD7763 is master and stm32f7 i...

EP.1 by Associate
  • 1875 Views
  • 3 replies
  • 0 kudos

Hello, I am making a CUSTOM HID Keyboard application with the stm32f103 processor, when I add the media keys (volume reduction, increase, etc.) to my project, the function that reads the status of the following leds with event_idx does not work. HELP!

this is leds status code ;static int8_t CUSTOM_HID_OutEvent_FS(uint8_t event_idx, uint8_t state){ /* USER CODE BEGIN 6 */if( (event_idx & 0x01) == 0x01 ){HAL_GPIO_WritePin(GPIOA,GPIO_PIN_10, GPIO_PIN_RESET);}else if( (event_idx & 0x01) != 0x01 ){HAL_...

AYılm.1 by Associate II
  • 1165 Views
  • 0 replies
  • 0 kudos

STM32F469 HID - add a keyboard to a custom HID

I have my custom HID device running and working fine. I would like it to also emulate a standard PC keyboard at the same time. So when my board enumerates, I would like the attached PC to find my custom device as well as a keyboard.I think I can ju...

Resolved! My STM32G473 has wrong flash size? How do I deal with this?

I have STM32G473VCT6 MCU. According to part number this device should have 256kB flash (Size code C). Flash size register (0x1FFF75E0) also shows 256kB (reg. value 0x100). However I can read and successfully write 512kB of data. STM32CubeProgrammer a...

tomaszuk by Associate
  • 3047 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.