STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L4Q5 GPIO hardware fault

I'm using STM32L4Q5CGUX on my project. I found some gpio errors. When I write on PB9, it's written on PB8. And I can't write on PB11. Could you guys check together, please?

DAC OUTPUT differs DAC 1 & DAC 2 on STM32F429ZI

Hi, I used STM32F429ZI​I want to check the output of DAC channel 1 and DAC channel 2.​But, the output of DAC channel 1 and DAC channel 2 were different.​HAL_DAC_SetValue( &hdac, DAC_CHANNEL_1, DAC_ALIGN_12B_R, 0 )HAL_DAC_SetValue( &hdac, DAC_CHANNEL_...

지한.1 by Associate II
  • 2366 Views
  • 8 replies
  • 0 kudos

Problems with HAL_I2S_Receive_IT

I need to receive I2S from from a device which digitises microphone audio and acts as an I2S masterI have use the STM32 Cube configuation tool to set I2S3 as a Half-Duplex SlaveWhen I callHAL_I2S_Receive_IT()I the code receives the callback into void...

Resolved! Received data not get into the variable

Hi everybody!I have an STM32F411RE Nucleoboard and an ADXL345-M accelerometer. I have 2 problems.I want to read 1 byte data from the accelerometer. In this case I want to get he device id (0xe5) and store it in a variable. In debug mode it seems that...

0693W00000Hp97aQAB.png 0693W00000Hp97VQAR.png
MSzal.1 by Associate II
  • 1943 Views
  • 2 replies
  • 0 kudos

Why FDCAN lose messages ?

I'm working on STM32L552RE. To read i use HAL_FDCAN_GetRxFifoFillLevel, and HAL_FDCAN_GetRxMessage. To write i use HAL_FDCAN_AddMessageToTxFifoQ.There is a mutex to avoid conflict. I don't understand why i'm loosing message when i write.Thanks for ad...

LDidi.1 by Associate
  • 846 Views
  • 0 replies
  • 0 kudos

STM32G0 Flash as EEPROM

Hi,I am working on STM32G071RB Nucleo Board and In one of project , I am using same MCU.In that Project , I don't want to use external I2C or SPI memory for saving the data (logs).1) How do I can access Flash as EEPROM ?2) Will this possible with STM...

STM32F303 ADC conversion time

Hi, I am using STM32F3Discovery board for our project at the moment. We need to sample 4 different signals at the same time so we are using all 4 available ADCs in parallel. We are triggering all the ADCs with Timer3 at 100kHz and to make sure the ti...

KHedi.1 by Associate II
  • 4667 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.