STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 H7 - SPI CLK behaviour at high frequencies

Hello everyone, I'm reaching out to seek guidance in pushing the SPI CLK line output to, at least, 65 MHz.In theory, this should be possible according to the Reference Manual by setting the GPIO speed to Very High in Vdd = 3.3. Currently, I am able t...

JCori_0-1757532686550.png
JCori by Associate III
  • 2081 Views
  • 9 replies
  • 5 kudos

Resolved! STM32F407 I2C Addressing Problem

Hello!I have a new project with a STM32F407VET6 and a STM32F103xxx over a RJ45 Jack with I2C.i worked a lot of time with I2C EEPROMs and it works fine, but my communication between the 2 STM's are horrible, or i am too confused.i found the tutorial o...

Sany by Associate III
  • 7211 Views
  • 12 replies
  • 2 kudos

Resolved! STM32U5A9J-DK1 USB Device question

I'm attempting to implement a USB MSC Device using the USB_OTG_HS on a STM32U5A9J-DK1. I'm using the STM32CubeMX version 6.14.1 and STM32Cube_FW_U5_V1.7.0 to create a USBX stand-alone (without THREADX) MSC device. The project builds and runs, with su...

OB programming issue on the custom bootloader

Hello,To protect the device's software, I am updating the RDP values in my own bootloader software, and to protect it in the event of a sudden power outage, I am also updating the BOR values. I am performing these updates only using HAL APIs. Additio...

pi_issue_2.png
neset by Associate II
  • 776 Views
  • 1 replies
  • 0 kudos

Resolved! SPI DMA STM32U031 wrong data

Hi everyone,Im currently trying to use SPI with DMA mode on STM32U031G6 with an S2LP,In this specific case I want to obtain the number of bytes present in my FIFO (10 bytes here), but the problem is that my reading through DMA mode does not work.Belo...

Quentin_27_0-1757497219651.png Quentin_27_1-1757497434702.png

STM32 CAN FD ISO Nominal 500kpbs Data 1Mbps

Hello,I am using STM32 microcontrollers on CAN FD ISO buses.The problem is that I am not able to configure CAN FD bus with a nominal rate of 500kbps and a data rate of 1Mbps. All others configurations are working as expected, see below all combinatio...

BBute.1 by Associate II
  • 1223 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G0 Engineering bytes programming

What is the sequence and APIs to erase and program the Engineering bytes?There are APIs to handle Main flash, and APIs to handle OTP, but it is not clear how the Engineering bytes should be handled.Thanks

STM32U031 SPI receive data of arbitrary length

Greetings!I am using the STM32U031 with STM32CubeMX HAL as an SPI Slave and would like to receive data that has variable length (max 50 bytes). I am using software NSS and my current approach is to start a DMA Rx/Tx transfer (using HAL_SPI_TransmitRe...

FlokRo by Associate
  • 1579 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.