STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32C011DxY, WLCSP12

I have a question about configuring pin D1 for UART1 TX (in conjunction with pin E2, UART1 RX).Pin D1 has the option for PA11, [PA9], PA8Pin E2 has the option for PA12, [PA10], PA71. To use pin D1 for UART1 TX, PA11 must be switched to PA9 (SYSCFG_CF...

ITEC by Associate
  • 469 Views
  • 1 replies
  • 1 kudos

Why STM32G473CBT6 program failed at 0x0800A000?

Hi there,I am using STM32G473CBT6, and work with a bootloader and application.When I set the application address at 0x08008000, everything works well.However, when I change the application address to 0x0800A000, the application download fails, except...

Junde_0-1758590452323.png
Junde by Senior III
  • 499 Views
  • 2 replies
  • 0 kudos

Internal Reference voltage VREF of STM32L4R9

Hi,I am using STM32L4R9ZIJ6 microcontroller.I have connected an external reference voltage of 3.3V to VREF+ pin and wanted to use internal reference voltage over this one for internal ADC read operation. Is that possible?I tried configuring the MCU t...

MoniR by Associate
  • 458 Views
  • 2 replies
  • 1 kudos

STM32U585 - Low Power Mode and UART DMA Issue

Dear STMicroelectronics Support Team,I am working with the STM32U585I-IOT02A development board, and I need assistance with the following:Entering and waking from low power modes (STOP2 or STANDBY) using the RTC wakeup timerConfiguring UART1 with DMA ...

shivss by Associate II
  • 876 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H753 CAN set up with both CAN-FD & CAN 2.0 frames

Hi, I'm trying to configure an STM32H753 FDCAN peripheral to be compatible with both CAN-FD & CAN 2.0 frames, in both the Tx & Rx directions.   How should I configure the FD-CAN peripheral to achieve this? I've been through he RM0433 document as best...

CZ_Home by Associate
  • 1051 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.