STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745I-DISCO – CAN TXFIFO Buffer Full Issue

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code. Hi everyone, I am working on Classic CAN comm...

Sumithra by Associate II
  • 2605 Views
  • 17 replies
  • 0 kudos

STM32N6 max power consumption versus GPIOs usage

New question from this thread. Hi @mƎALLEm  I am using STM32N6 Nucleo-144 board. In this board VDDIO is the power supplied at VDD, VBAT. VDDIO2, VDDIO4, and VDDIO5. So this the the power supply which is driving GPIOs. This power is generated by LD390...

GBA by Associate II
  • 753 Views
  • 2 replies
  • 2 kudos

STM32H750 QSPI External Flash Programming Fails

I'm using an STM32H750XBH6 MCU with two external Flash(W25Q256 X2) chips connected via QSPI. I followed the guide (W25Q FLASH Memory || Part 10 || QSPI & External Loader on H750) to create a custom external loader (.stldr) using STM32CubeIDE, and I m...

WayneLI by Associate
  • 872 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G431RB Internal Temperature Sensor

Hello, I am working on the STM32G431RB Nucleo board, specifically on the internal temperature sensor. I am facing issues in getting accurate readings. For your reference, I have attached: My code implementation An Excel sheet comparing temperature ...

Resolved! Thermistor reading error with ADC1

Post edited by ST moderator to be inline with the community rules especially with the code sharing. 1- In next time please use </> button to paste your code. Please read this post: How to insert source code. 2- Post is not related to CubeIDE usage b...

Resolved! Heartbeat pulse with DAC and Timer

I tried to search the forum so I'm sorry if there is a solution posted to this problem.I have been struggling with creating the pattern inside the image. Every 10 seconds I want a short heartbeat pulse generated by DAC. (DAC goes high, then low).The ...

paintspot_0-1758561651756.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.