2025-09-23 9:02 AM
I am working with an STM32N6 microcontroller and need clarification about the electrical characteristics of its GPIO pins. How much current a GPIO can source and sink. Is it in micro Amps or mili Amps.
Solved! Go to Solution.
2025-09-23 9:22 AM - edited 2025-09-23 9:23 AM
Hello @GBA and welcome to the community,
STM32N6 GPIO pin can source or sink up to ±20 mA.
From the datasheet page 172:
2025-09-23 9:22 AM - edited 2025-09-23 9:23 AM
Hello @GBA and welcome to the community,
STM32N6 GPIO pin can source or sink up to ±20 mA.
From the datasheet page 172:
2025-09-23 9:23 AM
20 mA source or sink. See the datasheet for details.
2025-09-23 9:56 AM
As the others have said, this is stated in the datasheet.
Note that there is also a limit on the sum total of all GPIOs ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.