STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C0 VREF+ Calculation

With a stm32c0116-dk, I am attempting to read vrefint, and calculate vref+. From my understanding of the data sheet, and schematic. VDDA is tied to VREF+ . On the development kit, these voltages are 3.3V.VREF+ = ((VREF _Charac+) * (VREFINT_CAL)) / VR...

pjhap by Associate
  • 869 Views
  • 1 replies
  • 0 kudos

STM32H7S7L8H6 Quad SPI - VDDXSPI supply voltage

Hello Team,We are planning to use STM32H7S7L8H6 in our design. With this part we want to integrate quad SPI Flash memory (Part Number :  W25Q128JVPIM with 3.3V Vcc).So, in STM32H7S7L8H6 VDDXSPI supply voltage 3.3V is ok, right? Thanks & Regards,Jigne...

JK1234 by Associate III
  • 566 Views
  • 1 replies
  • 0 kudos

USB DFU not work with RDP Level1

Hello Team,With RDP set to Zero Level , Firmware upload succesfully using CubeProgrammer GUI ( USB DFU mode ).But If I set RDP LeveL 1 , Device not able to detect on PC device manager and not able to connect with STM32 using CubeProgrammer USB interf...

bsuthar by Senior
  • 1297 Views
  • 7 replies
  • 0 kudos

Choosing package for STM32H743 SPI HS - BGA or LQFP ?

Hi,I'm interfacing external ADC - 16 bit, 10MSPS (AD7626) with this microcontroller. STM32 SPI will work in slave mode, ADC will provide 80MHz clock. It will work in a burst mode - sampling 288 measurements x 16 bits at 5MHz.I can't decide whether I ...

cipek by Associate II
  • 1817 Views
  • 11 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.