2025-09-28 9:39 AM - last edited on 2025-09-29 2:00 AM by Andrew Neil
Hi,
I'm interfacing external ADC - 16 bit, 10MSPS (AD7626) with this microcontroller. STM32 SPI will work in slave mode, ADC will provide 80MHz clock. It will work in a burst mode - sampling 288 measurements x 16 bits at 5MHz.
I can't decide whether I need BGA for this or LQFP will be sufficient. I remember having issues with internal ADC under performing when used in LQFP package. I don't want to go with BGA unless I have to.
Cheers
2025-09-28 10:42 AM
Check DS, H7 can get 133 MHz at max, no way to 250-300.
2025-09-28 11:55 AM
Could you elaborate on the speed please? Where did you get 133 MHz? I'm not familiar with DS, what is it?
2025-09-28 1:42 PM
DS = data sheet.
https://www.st.com/resource/en/datasheet/stm32h743vi.pdf
Table 106. SPI dynamic characteristics(1) page 192.
2025-09-28 2:21 PM
I haven't looked into that table, thanks. In the clock configuration I can set the SPI clock to almost 200 MHz. I was hoping that this would be enough for 80 MHz signal. At this point I don't see any other options other than FPGA.
2025-09-28 3:29 PM
I can't find any stm32 uCPU with serial LVDS interface supported. STM32CubeMX lists some STM32MP2xx where :
LTDC provide pixels to the LVDS display interface (LVDS).
specifically for LCD/TFT display, not serial data like SPI
2025-09-28 11:49 PM - edited 2025-09-28 11:53 PM
Hi,
the 80M SPI clock should be no big problem , but the AD7626 has LVDS interface : STM32 dont have this on SPI.
So you need LVDS -> cmos transceiver or a chip with native LVDS , typical a FPGA with LVDS here is suitable.
2025-09-29 3:09 PM
So is 80 MHz an issue here or not? I was going to use a LVDC receiver like ADN4662. I've seen completely different opinions on this subject.
2025-09-29 11:02 PM
If 80M SPI clock is the maximum you want, it should be no problem , with lvds receiver, short tracks, and damping resistors in all lines, maybe 33r .
I never tried this, my max SPI clock was 36 MHz, just for fun, to a TFT; using thin wires, free air, about 60mm long; was working fine, but more than double the given speed of the TFT, so reduced clock later, to avoid killing the TFT by overclocking.
2025-09-30 10:21 AM
@cipek wrote:So is 80 MHz an issue here or not? I was going to use a LVDC receiver like ADN4662. I've seen completely different opinions on this subject.
Better to ask on analog.com, I have hard time to comprehend theirs DS.
First read confuses me on :
CNV to Last CLK (LSB) Delay 72 ns max (page 6 adc DS), having 18 clk gives 4 ns and consequently 250 MHz minimum.
Than small print note 2 indicates that:
(tCYC − tMSB + tCLKL)/n
and page 3 points 0.1 msps minimum sampling rate, so clk may be as low as 0.1x18 = 1.8 MHz
Regarding H7 SPI I have tested up to 83 MHz, reading data out af ad7983 /84. Not LVDS, regular CMOS 3.3V
10 cm dupont cables, series resistance 470 Ohm
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.