STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can an ADC input read influence the encoder input ?

Hi!we use STM32G473 with 4 timers for 2 motors, for each motor we use 2 timers connected with ITR , the first timer is used as encoder input to hold the position, the second timer interrupts on each edge of of the encoders and calculate the speed.Wh...

0693W00000YAAegQAH.png
sde c.1 by Senior II
  • 2365 Views
  • 3 replies
  • 0 kudos

STM32L462 not found - ST-LINK V2 / V3 in STM32CubeIDE

Hi,I have STM32CubeIDE 1.7.0 issue whereby I can connect either ST-Link V2 or V3set to our custom board that has STM32L462RET6 MCU. Same with STM32 Cube Programmer - can't connect - target not found. Inside IDE, there's problem launching GDB serv...

MI.3 by Associate
  • 10662 Views
  • 11 replies
  • 0 kudos

Resolved! STM32F4 Disco RTC (old version) not updating SECONDS

I am using the Audio Playback and record exaample.I modified Systeem_clock_config as follos /* Enable HSE Oscillator and activate PLL with HSE as source */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI | RCC_OSCILLATORTYPE_HSE; RCC_...

shorai by Associate III
  • 2143 Views
  • 3 replies
  • 0 kudos

Problems with UART transfer using DMA on STM32L471RGT6

Hi , I am using DMA/serial port transfer with RTS /CTS handshaking to transfer between 490 and 506 bytes from variable dma_buffer. The byte stream is terminated with \r\n\0 . the code is below : while (transmit_complete_flag !=1 ){;} // wait here un...

rwils.1 by Associate III
  • 1576 Views
  • 1 replies
  • 0 kudos

RTC of smt32F103C8T6 is not incrementing time seconds while VBAT is connected to a 3v coin cell on VDD cut-off, but it only retains the last value but not increasing.

RTC code is not working properly while VBAT is connected to a 3v coin cell, it only retains time from the last value but not incrementing as the time increases please let us know what's wrong with the codeI'm following this below linkhttps://www.micr...

ashutamar by Associate II
  • 1653 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.