2023-02-06 10:14 AM
I want to made a simple Voice Recorder and Player Module, i found an interesting article here:
https://community.st.com/s/article/how-to-play-audio-files-using-stm32-part-1?t=1675535162773
But it´s focused to STM32G0, and i have stm32f401, i´have tried to follow the steps presented there, without luck...
So, i´ve decided, to make more simple (i think =/)
I know the stm32f401 only have adc, but not dac, so, i´ll use pwm to reproduce small audio´s, stores in internal memory
2023-02-06 12:41 PM
shure. just depends on : how much time will you invest and what quality you expect.
i made a audio player, plays wav or MP3 files from USB stick to a dac by I2S. (dac can be TDA1387 , some 30 ct . on Ali.)
i remember a program on an AVR (8bit, 20MHz) that records and plays back low quality audio just by using the pins and a R-C filter, some sigma-selta modulation without complex compression.
2023-02-06 1:21 PM
Thx for your answer AScha.3!
Initially, only want to do it, without extra periferialls, only internal memory, stm32f401 don´t have dac, only adc, for record some seconds with an analog mic, and reply later, via pwm, can you please, show me some link to the avr program?
2023-02-07 2:05 AM
it was long time ago...so i am not shure...maybe:
http://people.ece.cornell.edu/land/courses/ece4760/FinalProjects/s2005/ik48_ua22/mysite/sw_hw.htm
https://hackaday.com/2011/09/03/pic-based-voice-recorder/
https://320volt.com/en/pic16f876a-sandisk-sd-kart-ses-kayit-calma/
// Sound Recorder using SD card and PIC16F876A, by www.moty22.co.uk
//
// File will compile with the free Hi-Tech C compiler.
// Recording is done by the ADC using only the LSB. Bytes are written to the SD
// at the rate of 20KHz. It is similar to the format of .wav sound files.
// For playback CCP is used as a DAC (Digital to Analogue Converter).
#include <htc.h>
__CONFIG(LVPDIS & WDTDIS & UNPROTECT & HS);
#define CS RC0 //chip select input
#define Stop RB0 //stop pushbutton
#define Play RB1 //play PB
#define Rec RB2 //record PB
#define Pause RB3 //pause PB
#define RecLED RB5
#define errorLED RB4
unsigned long loc; //pause location
unsigned char SPI(unsigned char data) // send character over SPI
{
SSPBUF = data; // load character
while (!BF); // sent
return SSPBUF; // received character
}
char Command(unsigned char frame1, unsigned long adrs, unsigned char frame2 )
{
unsigned char i, res;
SPI(0xFF);
SPI((frame1 | 0x40) & 0x7F); //first 2 bits are 01
SPI((adrs & 0xFF000000) >> 24); //first of the 4 bytes address
SPI((adrs & 0x00FF0000) >> 16);
SPI((adrs & 0x0000FF00) >> 8);
SPI(adrs & 0x000000FF);
SPI(frame2 | 1); //CRC and last bit 1
for(i=0;i<10;i++) // wait for received character
{
res = SPI(0xFF);
if(res != 0xFF)break;
}
return res;
}
void InitSD(void)
{
unsigned char i;
for(i=0; i < 10; i++)SPI(0xFF); // min 74 clocks
CS=0; // Enabled for SPI mode
if (Command(0x00,0,0x95) !=1) errorLED = 1; // Reset SD command
while (Command(0x01,0,0xFF) !=0) {} //wait for idle state
SSPM1 = 0; // full speed 2MHz
CS = 1;
}
void WriteSD(void)
{
unsigned int r,i;
CS = 0;
ADON = 1;
RecLED = 1;
r = Command(25,loc,0xFF); //multi sector write
if(r != 0)
{
errorLED = 1;
ADON = 0;
RecLED = 0;
}
SPI(0xFF);
SPI(0xFF);
SPI(0xFF);
while(Stop && Pause)
{
SPI(0xFC); //multi sector token byte
for(i=0;i<512;i++)
{
GODONE = 1; //ADC input sample
while(!TMR2IF){} //20KHz clock
SPI(ADRESL); //send analogue byte
TMR2IF = 0;
//play while record
CCP1X = ADRESL & 1; //shift byte to get the required PWM duty cycle
CCPR1L = (ADRESL >> 1);
}
SPI(0xFF); // CRC
SPI(0xFF); // CRC
if((r=SPI(0xFF) & 0x0F) == 0x05){ //data accepted = 0101
for(i=10000;i>0;i--){
if(r=SPI(0xFF)) break;
}
}
else{
errorLED = 1;
}
while(SPI(0xFF) != 0xFF); // while busy
loc += 512;
}
SPI(0xFD); //stop transfer token byte
SPI(0xFF);
SPI(0xFF);
while(SPI(0xFF) != 0xFF); // while busy
CS = 1;
ADON = 0;
RecLED = 0;
}
void ReadSD(void)
{
unsigned int i,r;
unsigned char data;
CS = 0;
r = Command(18,loc,0xFF); //read multi-sector
if(r != 0)errorLED = 1; //if command failed
while(Stop && Pause)
{
while(SPI(0xFF) != 0xFE); // wait for first byte
for(i=0;i<512;i++){
while(!TMR2IF){}
data = SPI(0xFF);
CCP1X = data & 1; //shift byte to get the required PWM duty cycle
CCPR1L = (data >> 1);
TMR2IF = 0;
}
SPI(0xFF); //discard of CRC
SPI(0xFF);
loc += 512;
}
Command(12,0x00,0xFF); //stop transmit
SPI(0xFF);
SPI(0xFF);
CS = 1;
}
void main(void)
{
// unsigned char Pause = 0;
// unsigned int i;
loc = 512;
// PIC I/O init
TRISC = 0b10010000; // sck rc3, sdo rc5, sdi rc4, CS rc0, rc2 CPP1.
TRISB = 0b1111; // switches
RBPU = 0; //pullup on
RecLED = 0;
errorLED = 0;
//analogue init
CCP1CON = 0B1100; //PWM mode
PR2 = 100; //20KHz
T2CON = 0B100; //prescale 1, post scale 1, timer2 on
ADCON1 = 0B11001110; // Fosc/16, ch1, ref=Vdd, right just.
ADCON0 = 0B1000000; // Fosc/16.
//SPI init
SSPCON = 0B110010; //low speed osc/64(125kHz),enabled,clock idle=H
CS = 1; // disable SD
InitSD();
while(1) {
if(!Rec) WriteSD();
if(!Play) ReadSD();
if(!Stop) loc = 512;
}
}
2023-02-07 3:24 PM
Thx for your time AScha.3!!!
I'll check your suggestions!!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.