2023-02-07 4:40 AM
RTC code is not working properly while VBAT is connected to a 3v coin cell, it only retains time from the last value but not incrementing as the time increases please let us know what's wrong with the code
I'm following this below link
https://www.micropeta.com/video46
I made code using STM32cudeMX code is attached below
Thank you in advance!
2023-02-07 6:04 AM
LSI is in VDD domain, i.e. it is not running from VBAT when mcu is powered down.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.