Resolved! About QSPI example code with STM32H747I-DISCO
HiI have a STM32H747I-DISCO boardI want to test NOR Flash ( MT25QL512ABB8ESF-0SIT ) with Quad SPII didnot find an example code for it.Can I get an example code for NOR Flash with IOC file.
Ask questions, find answers, and share insights on STM32 products and their technical features.
HiI have a STM32H747I-DISCO boardI want to test NOR Flash ( MT25QL512ABB8ESF-0SIT ) with Quad SPII didnot find an example code for it.Can I get an example code for NOR Flash with IOC file.
Hi,I'm trying to get a clock output at 460.9 Khz on PB2 by setting the MCO2.The PB2 pin is declared as follow:static void MX_GPIO_Init(void){ GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOB_CLK_ENABLE(); /*Config...
void External_Clock_Config(){ TIM_ICInitTypeDef TIM_ICInitStructure; TIM_OCInitTypeDef TIM_OCInitStructure; NVIC_InitTypeDef NVIC_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); /...
Hi ,We have SEGGER J-TRACEpro for CORTEX-M processors . https://shop-us.segger.com/product/j-trace-pro-cortex-m-8-18-00/ We want to take the Code Coverage report . We are using Ozone IDE and loading the .OUT file to the OZONE IDE .There are 2 cables ...
When data size equal to 3 rx buffer last element is true only others are not. I expected all of them is true data. Why it is working like that ? I examine the result on debug modestatic void Init_SPI2(void) { SPI_InitTypeDef SPI_InitStructure; ...
If someone has that information please share, better would be if you can point me to the documentation where I can found the information. We are using the STM32F429ZI nucleo board.
Hello,I’m using STM32L412RB.I'm trying to differentiate between the types of chargersWhen the charger is connected, reboot occurs, and I run HAL_PCDEx_ActivateBCD()/HAL_PCDEx_BCD_VBUSDetect() in MX_USB_DEVICE_Init().After that, in case of abnormalit...
Hi,I am using the STM32L082 and looking for ways to have a watchdog implemented.However during long periods of low power sleeps (e.g. 12 hours) I would like to freeze the IWDG downcounter.Is this possible for the STM32L082? Thanks
Hello dear! I'm developing a new product. I would like use the STM32 F1 series, but I was surprised with this: https://blog.zapb.de/stm32f1-exceptional-failure/The F1 Series don't have RDP Level 2 protection, in this case, what's the most security wa...
I am planning to use ADC with 16 bits achieved using oversampling in STM32U5.But on Datasheet there is no data wrt to ADC oversampling.Can somebody help me with data regarding ENOB, EL,ED when ADC is oversampled. Datasheet : DS13737Datasheet - STM32U...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.