STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeProgrammer - no st-link detected (win7)

ST-LINK V2 works fine with STM32 ST-LINK Utility and STM32CubeIDE, but ST-LINK V2 doesn't work with STM32CubeProgrammer.Any idea why this might be? I have tried various USB ports and various USB to mini USB cables. I am using original programmer and ...

Resolved! STM32 L412 Timer interrupt not working

I am using STM32L412 microcontroller and doing baremetal programming for timer interrupt. I am using Timer 6 and base clock of 4MHZ is used as HCLK. However my interrupt is not firing below mentioning my code. count variable is also not updatingint m...

SSaiy.1 by Associate III
  • 6781 Views
  • 14 replies
  • 0 kudos

Restart without Register RCC->CSR bits set (STM32F417ZGT6)

Hi there,we have an application which already tracks register RCC->CSR on startup and writes the content to the log files.From time to time, due to (intentionally unfiltered) electrical disturbances in the electronic or external EM pulses, we see the...

Ingmar by Associate II
  • 708 Views
  • 0 replies
  • 0 kudos

I want to write a program for the STM32F303VC board that uses SPI interface to make a comunication between the MCU and the L3GD20 gyroscope and read the values of the 3 axis.

The results are always the same: x=-6.145, y=-6.149, z=-6.149 , even if I move my board. What's wrong?#include <stm32f30x.h>void GPIO_Config();void SPI_Config();uint8_t L3GD20_Read(uint8_t reg);void L3GD20_Write(uint8_t reg, uint8_t data);void L3GD20...

FPalo.1 by Associate II
  • 1187 Views
  • 1 replies
  • 1 kudos

Problems with folder .c and .h configuration

Hello everybody,I'm a newbie in stm32 IDE. I come from microchip 8bit PIC world :)For a small personal project I would like to use a SIM800 GSM module with an STM32F303.in order to make my code clear I would have liked to break it down into several p...

JJoao.1 by Associate III
  • 1504 Views
  • 2 replies
  • 0 kudos

Resolved! Analog Watchdog to trigger on offset adc value

I am applying 4 offset to 4 adc channels and calculating the analog watchdog high threshold based on a threshold above the highest adc channel. The purpose of the adc offsets is to equalize the channels readings, such that the adc watchdog high thres...

KLW by Associate
  • 2245 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.