STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use SWV logging without SWO pin?

Hi all,I have custom hardware in the G4 series (491RE) and want to log some data. I don't have any communication method accessible now. Only I can access SWDCLK and SWDIO pins. SWO pin used for another purpose. is there any method where I can get SW...

Roshan by Associate III
  • 3873 Views
  • 3 replies
  • 1 kudos

Multiple images

Regarding STM32G0B1In a remotely operated AUV I would like to have a mechanism for two or more full code images with the option of rollback. 1) Is it possible to partition main FLASH in two with a selection mechanism and rollback2) Ist it possible to...

JSorl.1 by Associate
  • 1342 Views
  • 1 replies
  • 1 kudos

STM32G4 Comparator Blanking Pulse (frequency change possible?)

Hello,I am using the comparators (COMP2) on STM32G4 and want to add some blanking windows to let the COMP2 input get rid of the system switching noise.The technical manual gives a very brief example as shown in Fig.1.  But I need something more compl...

0693W00000Y959vQAB.png 0693W00000Y95AAQAZ.png
QMa.1 by Associate
  • 2291 Views
  • 1 replies
  • 0 kudos

Hello every i have One doubt in stm32 Im send the frame formate in Docklight but I cant able to check my frame .anyone give the solution

Hello every I have One doubt in stm32 I am send the frame formate in Docklight but I cant able to check my frame using without interrupt .anyone give the solution/* USER CODE BEGIN Header */ /** *****************************************************...

0693W00000YAaJuQAL.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.