2023-02-13 10:16 AM
Hello everybody,
I'm a newbie in stm32 IDE. I come from microchip 8bit PIC world :)
For a small personal project I would like to use a SIM800 GSM module with an STM32F303.
in order to make my code clear I would have liked to break it down into several parts. But I admit that I don't really understand how to do things right.
For example I would like to make a gsm.c file and therefore a gsm.h only for the GSM part. In order to put the functions concerning the gsm part.
But here I need to use the UART library in the main.c and also in the gsm.c, is this possible and how to do it and declare it?.
In addition I would like to have variables that can be common to both .c files, is this possible?
Thank you for reading me
2023-02-13 4:23 PM
This has nothing to do with STM32 - you just have to learn the C language, compilers and software development in general.
https://stackoverflow.com/questions/47919/organization-of-c-files
2023-02-13 6:49 PM
True, the base C coding will be required to get the job done.
In C, there are header file (the name and constant/define declarations), which will be shared (included) among source code C files. And for USART, I would suggest to look at LL (low layer) code example for the nucleo F303 to start from a compiling project.
As for global variables, you declare them in a C file and you can use them wherever you declare them as "extern uint32_t myVar;"
One piece of advice : If you use a global variable in a function, pass the global variable as function passing parameter. Your function will remain reentrant and multi-core/multi-thread safer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.