2023-02-13 5:05 AM
ST-LINK V2 works fine with STM32 ST-LINK Utility and STM32CubeIDE, but ST-LINK V2 doesn't work with STM32CubeProgrammer.
Any idea why this might be? I have tried various USB ports and various USB to mini USB cables. I am using original programmer and original windows 7 x64 version.
On another PC with windows 10, the same programmer works in STM32CubeProgrammer.
What should I do to get ST-LINK V2 to be seen by STM32CubeProgrammer?
If you need any additional information, I am ready to provide it.
2023-02-13 1:52 PM
Is the ST-Link connected to USB 2.0 port or USB 3.0x? If the latter, try to connect it to USB 2 port or external USB 2 hub.
2023-02-13 8:22 PM
I tried connecting ST-link to both USB2 and USB3. Tried the front and back of the PC. I also tried to connect through the hub. The result is the same, the programmer works with STM32CubeIDE and STM32 ST-LINK Utility, but does not work with STM32CubeProgrammer.
2023-02-14 12:56 AM
just from my experience with win10 -> mysterious problem :
it could be about the "rights" you have (or give to the progam) to access the hardware.
try to change the "rights" or just try start prog as "admin".
2023-02-14 1:08 AM
On windows 10 everything works fine for me.
On windows 7 I tried to run as administrator, still no st-link detected.
2023-02-14 1:43 AM
a pity . my last idea : any kind of anti-virus program running?
2023-02-14 2:29 AM
I have kaspersky antivirus installed. After turning it off, nothing changes either, everything is still no st-link detected. I think it's something else, but I can't figure out what...
2023-02-14 2:38 AM
And new instalation CubeProgrammer?
2023-02-14 3:23 AM
Of course I tried. Still no st-link detected...
2023-02-14 3:36 AM
can you test with another STlink, maybe V3 , or a nucleo board (with onboard link)?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.