STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 A/D Input Bias Current

I'm not able to find a spec in the STM32F446 datasheet for minimum A/D input bias current. Does anyone know where I can find this info? I need to sample the voltage from a high resistance potentiometer and it would be handy to know if I need to buf...

Resolved! Output Capture not working to blink LED on NUCLEO-C031C6

I am trying to implement output capture using the LL APIs but cannot get it to blink the LED every one second on the NUCLEO board, however, I cannot get it to blink at all. Is there a register I missed?Here is my code:#include "stm32c0xx_ll_bus.h"#in...

HPate.12 by Associate II
  • 3975 Views
  • 7 replies
  • 0 kudos

Discovery L0538 UART2 RX Pin Stuck Low?

Using a Discovery L0538, and want to make use of the 2nd UART (really only need the RX on pin PA3). I noted in the User Manual that to disable the onboard touch sensor and use this pin, I need to jump solder bridge SB24 (which I did, alng with the ot...

0693W00000aHd0XQAS.png
nobbyv77 by Associate II
  • 6052 Views
  • 14 replies
  • 0 kudos

Resolved! ST BLE Toolbox: How to use the environment

Hello,I am working with the Nucleo Bluetooth boards (NUCLEO-F401RE + NUCLEO-IDB05A2) and I want to test some custom code I'm writing to make sure I understand how to use the X-CUBE-BLE software package. To do this, I am trying to use the ST BLE Toolb...

KMew by Senior III
  • 1946 Views
  • 1 replies
  • 0 kudos

Resolved! STM32C031C6 Timer Input Capture

I'm attempting to do a simple Input Capture using Timer1. I thought as a start I would generate a single 200uS pulse using a Signal Generator and use Timer1 to detect it. I can't seem to get the capture to work no matter what I do.I tried using HAL a...

MHank.1 by Associate III
  • 2690 Views
  • 2 replies
  • 0 kudos

Resolved! DFSDM Output resolution

When I use DFSDM, I configure FOSR= 256 ISOR=1 and the output is outside the range in the reference guide +-16777216

GWenJ.1 by Associate II
  • 2905 Views
  • 4 replies
  • 0 kudos

In the case of STM32U575ZIQ, Can I use an external DMA (and not the internal I-DMA) to interface the SDMMC card?

Basically, when I use the IDMA of STM32U5, there is a significant delay happening while communicating with the card. And if I do the same by using STM32F4(which uses general DMA), then there is not such a huge delay. After checking other parameters (...

ANalg.1 by Associate II
  • 1610 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.