STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC output suddenly becomes constant

Hello,I'm using the ADC on a STM32G431 to read 5 voltages at 20kHz. Everything works well, but suddenly the 5 channels "get stuck" or freeze, i.e. the value they measure becomes constant even though the voltages on the input pins still fluctuate. Som...

ikrosoft by Associate II
  • 10333 Views
  • 12 replies
  • 0 kudos

Resolved! customized PCB with STM32F7 series uController can not be seen by any STM programs(ie. STM32Cube programmer, STMCube IDE, St utility ...)

After changing some properties, those are: -"BOR_LEV" set up 1 (BOR Level 2 VBOR2 brownout threshold level 2) -"RDP" set up CC (level 2 chip protection) from "Option Bytes" segmentation in STM Cube Programmer(It was unintentional case and before th...

I2C is not sending a repeated start

Hello. I encountered a problem. I have an STM32F103C8T6 controller and I am trying to implement I2C communication using interrupts. The problem is that when I need to send a repeated start, it doesn't happen. ITBUFEN interrupts are disabled, I only u...

RSolo.1 by Associate II
  • 2443 Views
  • 2 replies
  • 0 kudos

Resolved! wrong UART interrupt is getting fired

I am using UART to transmit and receive data. for transmitting I am using polling method function HAL_UART_Transmit(&hart1, buf, 8,1000) and for receiving i am using HAL_UART_Receive_IT(&hart, Rx_buf,8); receiving is working fine but after transmitti...

Anwar.786 by Associate II
  • 5468 Views
  • 17 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.