2023-02-27 4:20 AM
Basically, when I use the IDMA of STM32U5, there is a significant delay happening while communicating with the card. And if I do the same by using STM32F4(which uses general DMA), then there is not such a huge delay. After checking other parameters (transfer block size, I-cache, D-cache, etc) I suspect that, if I use the external DMA then, will the delay issue gets solved.
In the ref manual, I do not see the GPDMA request along with SDMMC.
So, please inform me if I can use GPDMA to configure the SDMMC and suggest your views on the mentioned issue.
2023-03-02 1:00 AM
Hello @ANalg.1 and welcome to the community,
You can refer to this Fimeware example : "STM32Cube\Repository\STM32Cube_FW_U5_V1.1.1\Projects\STM32U575I-EV\Examples\SD\SD_ReadWrite_DMALinkedList"
And also there is the how to use the GPDMA for STM32U5 application note
Aymen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.