2023-03-01 7:42 PM
2023-03-01 11:28 PM
Welcome, @SNC.1, to the community!
Well, if you've deleted everything, everything is deleted. It's like an audio CD - if you take it out of the player and shred it, the player can no longer play the music. Accordingly, the MCU can't know what to do and how to control the display.
Is it your own board or a DISCOVERY?
Regards
/Peter
2023-03-02 9:20 AM
It's a DISCOVERY board which was given by my senior executive.
If there is any chance to recover the erased memory from STM32F746, Because next I have to do vocoder project using this MCU.
2023-03-02 9:41 AM
Download the CubeF7 V1.14.0 package, the original demo firmware is in there.
STM32Cube_FW_F7_V1.14.0\Projects\STM32746G-Discovery\Demonstrations\STemWin\Binary\STM32746G-DISCO_Demo_V1.5.0.hex
2023-03-02 10:06 AM
2023-03-02 12:15 PM
@Community member has provided you with the original software, but you would only need it to restore the original state. If you put a new program on it, the original software will be overwritten anyway.
In order to see something on the LCD, you would of course also have to program the LCD graphically in your own programme, e.g. using TouchGFX.
Regards
/Peter
2023-03-02 12:25 PM
This and related PM's, probably suggest confusion about why the screen isn't doing anything when there's no code to configure it, and the OP's concern that this is now broken.
I think the initial goal is to go back to something that does work, and illustrates that the board is not physically broken.
Getting something built and working independently seems like the next hurdle..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.