STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo F401R1 - Timer interrupt and lockup

 I am using timer interrupts to read 2 optical encoders connected to 2 motors. Everything seems to run fine for a while, then I get a hard lockup and everything stops. The time can be 5 minutes or 2.5 hours. I installed and setup watchdog and when it...

THoyl.3 by Associate
  • 2190 Views
  • 3 replies
  • 0 kudos

For STM32L4S5, how to access the calibration register and how to calculate what values to store in that register? We're having a problem with the calibration of the real-time clock. It's significantly off-time over a period of several days.

We believe there is a register setting to calibrate it, how can we debug this issue please? What are the steps to calculate the calibration register value and how do we get them into the register?

EHD by Associate II
  • 2100 Views
  • 5 replies
  • 0 kudos

NUCLEO-C031 Pin Change interrupt not firing

[Update]Seems you can't mix C and C++ files easily, so I converted the main file to C and everything works fine. [/update]I am attempting to do what I thought would be a simple pin change interrupt on PB0.I set up the pin change in HAL and it works, ...

MHank.1 by Associate III
  • 1370 Views
  • 1 replies
  • 0 kudos

STEVAL PROTEUS-1 - Modal analysis using impact hammer

Dear all, I'm trying to evaluate the IIS3DWB sensor using the STEVAL PROTEUS-1. Would it be possible to use the sensor to capture transient vibration e.g. Modal test using an impact hammer? Is there an example script for STEVAL PROTEUS-1, to capture ...

Ravide by Associate
  • 819 Views
  • 0 replies
  • 0 kudos

STM32F030CC Bootloader application stuck at first HAL_Delay

Hi, I am working on STM32F030CC microcontroller, where I am calling an application code from bootloader code. When the code is entering the application, the program is entering into an infinite loop of HAL_Delay(). I found out that by adding "SCB->VT...

JObbu.1 by Associate
  • 1369 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.