2023-03-29 4:28 PM
Dear all, I'm trying to evaluate the IIS3DWB sensor using the STEVAL PROTEUS-1. Would it be possible to use the sensor to capture transient vibration e.g. Modal test using an impact hammer?
Is there an example script for STEVAL PROTEUS-1, to capture the data and save it to an SD card? The trigger signal will be manually activated prior to the impact and the data will be captured for 60 - 90 seconds. The sampling rate will be a min. of 20kHz as the highest frequency of interest is approx. 7kHz. Any advice would be much appreciated.
Thanks in advance,
best regards,
Ravi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.