STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SRC236/441 libs with Hard FPU support?

I believe all of the audio processing addon libs, (SRC236/SRC441) are built without hardware FPU support. The problem is my entire project was built with hard FPU support. I tried the mixed SW/HW, but that didn't solve the issue and I couldn't build ...

Zaher by Senior II
  • 2569 Views
  • 3 replies
  • 1 kudos

Communication with STEVAL-MKI109V3 kit

I would like to use STEVAL-MKI109V3 with LSM6DSV16x Imu sensor. I have other tools like ESP32 and some sensors that controls autobrake system based on IMU data. I communicate between ESP32 and PC(Python) through BLE. However, if I add STM32F401VE. th...

FKara.3 by Senior
  • 773 Views
  • 0 replies
  • 0 kudos

Resolved! SPI Signal Shape Issue

Hello,I am try to control an external DAC system with the SPI interface. The clock signal shape looks like the attached file. I didn't figure out the meaning of the signal. Yellow is the clock signal and the blue is CS signal.

0693W00000aJE10QAG.jpg
AE104 by Senior
  • 7545 Views
  • 24 replies
  • 0 kudos

Bit Banding issue

I have an issue with using bit banding on stm32U575ZI-Q board when I want to write on it Hard fault is appear what is the problem and How to overcome this issue?

rsoli.1 by Associate II
  • 2535 Views
  • 3 replies
  • 0 kudos

Resolved! (SOLVED) STM32H743ZIT6: Bad accuracy of TIM2 (32Bit Timer)

Hello,I am having accuracy issues on TIM2 (32Bit Timer). I am feeding the PLL with an HSE 32MHz crystal (which seems to be fine when I measure the MCO frequency). I have setup the Prescalers to reach a frequency of 240MHz for the APB1 Timer clocks (w...

0693W00000aPOKxQAO.png
JArig.1 by Associate II
  • 1615 Views
  • 1 replies
  • 0 kudos

Resolved! Stop mode is woken by another EXTI line

STM32L071CBT wakeup power button PC13, PWM signal = PA11I have a device that wakes every 20 seconds then goes to sleep, it can also wake when the power button is pressed, part of it's wake cycle it to check the servoInt pin for activity.pin setup /*C...

markH by Associate III
  • 2591 Views
  • 4 replies
  • 0 kudos

When one does ADC oversampling, what should be the sampling time?? Higher sampling time or lower sampling time will give better results??

i am working on ADC oversampling using STM32 nucleo board. I have increased 2 bits by using appropriate oversampling ratio and bit shifting. But when i used lower sampling time i observed less % error between expected v/s measured ADC count then high...

STee.3 by Associate II
  • 3279 Views
  • 4 replies
  • 0 kudos

STM32F411 - temperature sensor returning 0

Hi All , Im trying to read the temperature from the internal temperature sensor.But everytime Im reading i recevied 0Here is my code:#define ADC1EN (1U<<8)void temp_init(){ // Configure ADC module ADC1_IN18 channel // Enable Clock access RCC->APB2ENR...

Tmizr.1 by Associate II
  • 3509 Views
  • 6 replies
  • 0 kudos

How can I read 4 inputs of ADC continously (using HAL)

I have initialized ADC1 and assigned it 4 channels (PA4-PA7 as IN4 to IN7). My initialization looks like this:static void MX_ADC1_Init(void) {   /* USER CODE BEGIN ADC1_Init 0 */   /* USER CODE END ADC1_Init 0 */   ADC_ChannelConfTypeDef sConfi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.