Resolved! STM32H5 - why only 250 MHz?
Why there's no 480..500MHz variants of H5, like in the H7 line?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Why there's no 480..500MHz variants of H5, like in the H7 line?
Hello all,I'm currently implementing a double async circular buffer on a STM32L432KC Nucleo board. In order to increase the flow speed of the data leaving the buffers, I'd like to change the FLASH wait states (i.e. set the wait state value to 0). The...
On STM32F407V-Disc the divisions don't work out for an 192KHz Timer trigger for the ADC, so sampling runs a bit slower or faster, the problem is that the Cirrus DAC audio chip cannot be set to match the sample rate, so I get buffer sync drift, audio ...
I have as simple MENU where I am switching with rotating of rotary encoder between items. If I choose item which I want I can press the button and it open subitem for the item. in open subitem I have stopped rotating of encoder. Because if I was in s...
We want to use external 16 bit SDRAM for heap and stack. The SDRAM is configured with byte enable and MPU. I tried to map the memory to 0xC0000000 and 0x60000000, but it doesn't matter. Also the configuration of MPU with MPU_TEX_LEVEL0 or MPU_TEX_LEV...
I tried the same code on both microcontrollers, but STM32F103RET6 freezes with NVIC_SystemReset(); Can you help me please?
Edge-triggered interrupts had been used by us to identify various system states. However, it appears that the interrupts are now sometime erroneous and cause an undesirable state change. This led us to search for implementations where level-triggered...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.