2023-04-23 9:32 AM
Hello all,
I'm currently implementing a double async circular buffer on a STM32L432KC Nucleo board. In order to increase the flow speed of the data leaving the buffers, I'd like to change the FLASH wait states (i.e. set the wait state value to 0). The ST documentation mentions the ART accelerator but does not provide enough details... I've also noticed a few code lines referring to wait states in the HAL_Init function.
Could someone explain how to implement that and which file(s) to modify?
I deeply appreciate your help!
Solved! Go to Solution.
2023-04-23 10:52 AM
The flash lines (256-bit) likely run about 50-60 ns, so a wait-state for every 16-20MHz
Subsequent word fetches within the line have zero cost, similar for anything in the cache
https://www.st.com/resource/en/product_training/STM32L4_Memory_Flash.pdf
The caching is quite efficient as it has an expedited path. For fast/predictable code execution you could put code in RAM.
2023-04-23 10:52 AM
The flash lines (256-bit) likely run about 50-60 ns, so a wait-state for every 16-20MHz
Subsequent word fetches within the line have zero cost, similar for anything in the cache
https://www.st.com/resource/en/product_training/STM32L4_Memory_Flash.pdf
The caching is quite efficient as it has an expedited path. For fast/predictable code execution you could put code in RAM.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.