STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1 ADC DMA multichannel

Having some trouble with reading ADC channels on this unit only when using multiple channels. I have no problem using a single channel, but as soon as I expand it to two, or more, my readings are just garbage.Code for working single channel: hadc1....

Resolved! ADC conversion data to DMA without any DMA interrupt ??

Hello team am Receving 16bit ADC conversion data to DMA in STM32H745i Disco in CubeIDE software. Here DMA interrupt is generating by default in software (i am disabled the interrupt in programming after that program counter is out of control) I dont ...

SA  V.1 by Senior
  • 7370 Views
  • 19 replies
  • 0 kudos

STM32H730 FDCAN TxDelayCompensation

I use FDCAN in STM32H730 for communication over CAN-FD.At the moment it works with 500kBit/2000kBit without TxDelayCompensation. But we want to communicate with 1000kBit/4000kBit too. Therefore I want to enable TxDelayCompensation.I'm not sure how I ...

Resolved! NUCLEO-U575ZI unable to activate PWM pin output

Hi everybody! I keep trying to out a PWM signal, using TIM1 ch1. CC do trigger fine, but the output pin doesn't change. Please help!void TIMER_init(void){ //PA8 - CH1 GPIOA->MODER &= ~((3 << GPIO_MODER_MODE8_Pos) + (3 << GPIO_MODER_MODE9_Pos)); //Sw...

Skfir by Senior
  • 1410 Views
  • 2 replies
  • 0 kudos

Resolved! ADC3+DMA

I'm having trouble with my STM32h757 processor. I'm trying to sample 2000 samples using ADC3+DMA1/DMA2/BDMA, but it's not working as expected. I set up the ADC to work in continuous mode and the DMA to work in circular mode with the address increment...

MDali.1 by Associate
  • 2196 Views
  • 3 replies
  • 0 kudos

Sync protocol on timers - Nucleo STM32L412KB

Hi guys,I'm "trying" to establish a STABLE communication between USB FX2LP sync slaveFIFO and STM32 MCU, in particular with the STM32L412KB for now.I need a stable data transfer from STM32 DMA-GPIO to FX2LP slaveFIFO with DMA clock 3MHz (later higher...

SSher.3 by Associate III
  • 4727 Views
  • 2 replies
  • 0 kudos

Resolved! I appreciate to guide me for ADC

I am usinghttps://os.mbed.com/platforms/ST-Nucleo-L496ZG-P/#board-pinoutwith this manualhttps://www.st.com/resource/en/user_manual/um2179-stm32-nucleo144-boards-mb1312-stmicroelectronics.pdfNow I would like to learn Analog-to-Digital Conversion (ADC)...

CG3 by Associate III
  • 2409 Views
  • 3 replies
  • 0 kudos

Resolved! OctoSpi in QuadSpi mode

​Hello,​I am trying to access an external flash memory (32 mbit) using stm32L4. Stm32L4 has OctoSpi. i have configured the OctoSpi with dual quad disabled but yet, i am not able to access the external flash mem. The external flash memory supports sin...

hp26 by Associate II
  • 2733 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.