STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interference between GPDMA channels on STM32U575

Hello,I'm trying to configure the GPDMA1 to transfer conversion results from ADC1 and ADC4 to two results buffers using two separate GPDMA1 channels on a STM32U575. The DMA channels are both configured as 'Standard Request Mode' with 'Circular Mode' ...

WTreh.1 by Associate
  • 1624 Views
  • 0 replies
  • 0 kudos

Help with understanding UART interface

I have a device made of two modules. Each module has its own ST microcontroller, family is STM32L476. They are connected together with a cable of 2-2.5 meter coated, most likely, with a silicone tube.I need to make the two microcontrollers communicat...

mdiro by Associate III
  • 6046 Views
  • 9 replies
  • 0 kudos

Resolved! STM32F730xx ADC: EOC never set when reading VREFINT

Hello,we want to read VREFINT to make our ADC measurements more accurate.But the EOC bit is never set when selecting the ADC_CHANNEL_VREFINT channel.PCLK2 is at 108MHz but ADC prescaler and sampling cycles are at max. so we assume there is no problem...

rengl by Associate II
  • 3390 Views
  • 6 replies
  • 0 kudos

Resolved! Bug Report: STM32 H723ZG wrong register name, FTHVL <-> FTHLV

In some places the register name "FTHLV" is typed wrong:The right register name is "FTHLV": In STM32 CubeIDE the name is wrongly spelled "FTHVL": In the Reference Manual RM0468 (Page 2227) it is one time called "FTHLVL": And in another Diagram (Page ...

_legacyfs_online_stmicro_images_0693W00000bimMBQAY.png _legacyfs_online_stmicro_images_0693W00000bimMkQAI.png _legacyfs_online_stmicro_images_0693W00000bimMzQAI.png _legacyfs_online_stmicro_images_0693W00000bimNJQAY.png
DBeck.7 by Associate
  • 3534 Views
  • 2 replies
  • 0 kudos

Resolved! Issue with the RTC REF_IN on STM32F439NIHx

Hi,I'm having some trouble with trying to correct the RTC drift on a STM32F439NIHx. I've enabled the REF_IN and provided a 50Hz signal on the pin, but the RTC still drifts by around 1s per day.I've also tested that the 50Hz signal is correctly receiv...

DPitt.2 by Associate II
  • 5891 Views
  • 17 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.