STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Not getting SPI connection between OV5642

The setup was tested with a arduino platform with the Arducam's github code. The entire working of Camera right from Capturing images to videos from the module(OV5642).Now I want to migrate to STM controller with the same camera module.I'm using STM3...

_legacyfs_online_stmicro_images_0693W00000bj381QAA.png
RAnan.3 by Associate III
  • 1369 Views
  • 0 replies
  • 0 kudos

I have a array declared as: char* arrs[20][30]; I have filled up this array with name and value and now I must compare for example, the first element of arrs [] value and the third element of arrs[] value. How can I do this?

I have tried to use strcmp and have also tried (arrs[0] == arrj[1][8]) with no luck. My goal is to check if the corresponding values are equal. (for reference: arrs[0] = freq :100kHz and arrj[1] = freq: 100kHz). I just wanted to see the values are e...

cjaya.2 by Associate II
  • 1281 Views
  • 1 replies
  • 0 kudos

How to solve this hardfault concerning memory access restriction?

The code goes toHAL_I2S_Receive_DMA at __HAL_UNLOCK(hi2s);andvoid HAL_DMA_IRQHandler(DMA_HandleTypeDef *hdma){ uint32_t tmpisr; __IO uint32_t count = 0; uint32_t timeout = SystemCoreClock / 9600; /* calculate DMA base and stream number */ DMA_Base_Re...

jess by Associate II
  • 2044 Views
  • 2 replies
  • 0 kudos

STM32F4 Nucleo board TIM1 stays high after DMA is finished

I'm using DMA with TIM1 to drive a string of WS2812B LEDs. I am closely following a tutorial called Controlling Neopixels with STM32 on Digikey (I cannot add links due to the age of my account) with some adjustments, with my ARR being 89, my clock be...

_legacyfs_online_stmicro_images_0693W00000binXoQAI.png 0693W00000binZQQAY_image.png
DAbdi.1 by Associate II
  • 6052 Views
  • 13 replies
  • 0 kudos

STM32L452CC and STM32L4Q5CGU6, issue with USART

My colleagues went to my office and reported that the STM32L452CC with the USART interface (5MHz and 10MHz) was working fine but had to use STM32L4Q5CG due to stock usage, but it failed at 10MHz but working fine 5MHz.I have explored errata, datasheet...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.